LPC1833 EEPROM reading

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1833 EEPROM reading

ソリューションへジャンプ
1,746件の閲覧回数
michaelershov
Contributor I

Hello, 

If I store important information in EEPROM; Flash protected from reading. Anyone can erase only Flash and write new code for reading EEPROM?

 

Best regards

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,456件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Michael Ershov,

In general, the Flash and EEPROM are independent peripherals, if the enable code read protection don't interfere the EEPROM operation.

So it's available to achieve your purpose.
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,457件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Michael Ershov,

In general, the Flash and EEPROM are independent peripherals, if the enable code read protection don't interfere the EEPROM operation.

So it's available to achieve your purpose.
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信