LPC1833 EEPROM reading

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1833 EEPROM reading

Jump to solution
1,766 Views
michaelershov
Contributor I

Hello, 

If I store important information in EEPROM; Flash protected from reading. Anyone can erase only Flash and write new code for reading EEPROM?

 

Best regards

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,476 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Michael Ershov,

In general, the Flash and EEPROM are independent peripherals, if the enable code read protection don't interfere the EEPROM operation.

So it's available to achieve your purpose.
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,477 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Michael Ershov,

In general, the Flash and EEPROM are independent peripherals, if the enable code read protection don't interfere the EEPROM operation.

So it's available to achieve your purpose.
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply