LPC1830 Boot Rom error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1830 Boot Rom error

ソリューションへジャンプ
2,409件の閲覧回数
koenvanderaa
Contributor II

Hi,

 

We are making a new product with the LPC1830. If i test my software on the LPC-Xplorer demo board everything is fine. But now it should work on our own PCB. 

 

I use LPCXpresso if i start the debugger the flash is programmed without a error. But the debugger stops at address 0x10406a0c. This is in the 64kB ROM of the chip. This part is responsible for the startup of the chip.

 

I configured the boot resistors to SPIFI so this could not be the issue. Also al the pins i can measure are going high and not tri state. Is this maybe the problem? 

So if somebody ever saw the same problem or if there is a engineer from NXP how knows what is happening on this address please help me.

 

 

Regards, 

 

Koen Van der Aa

タグ(2)
0 件の賞賛
返信
1 解決策
2,207件の閲覧回数
koenvanderaa
Contributor II

Hi, 

The problem is ok now. we had pin 2_7 connect to the GND because of this the chip went in to UART boot mode but we do not want this. 

Thanks! 

Koen Van der Aa

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,208件の閲覧回数
koenvanderaa
Contributor II

Hi, 

The problem is ok now. we had pin 2_7 connect to the GND because of this the chip went in to UART boot mode but we do not want this. 

Thanks! 

Koen Van der Aa

0 件の賞賛
返信
2,207件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Koen Van der Aa,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

I'm a bit confused with this issue.

At first, you mentioned that your software can work well on the LPC-Xplorer board, however you said that the debugging operation has some troubles.

So I was wondering if you can describe the issue in more details, and I will appreciate if you share some screenshots.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信