LPC17xx RTC not reliable within temperature spec

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC17xx RTC not reliable within temperature spec

2,213件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by probatista on Thu Mar 13 06:27:39 MST 2014
Both the LPC175x and LPC176x errata sheets report an issue with RTC reliability: "The Real Time Clock (RTC) does not work reliably within the temperature specification".

1. Since this issue is said to affect only revisions "Rev A" and "-", I want to buy a newer revision. The Errata sheet explains how to read the revision from the top marking, but I'll buy it on the internet and therefore will not be able to read it. How can I know which revision is the device I will buy without reading its top marking? Does the 551 on this manufacturer part number "LPC1756FBD80,551" says something about it? I'm thinking about buying this: http://br.mouser.com/ProductDetail/NXP/LPC1756FBD80551/?qs=%2fha2pyFaduifPp1Rdf3p9P0nsUa%252bPB82arX...

2. Are there any more details about this issue? Problems only occur on extreme temperatures (next to the device limits)? If my application will only operate from 10 to 40 degC should I expect any problem? This issue will only cause small delays or might even stop the RTC?

Thanks in advance, any help is appreciated.
Paulo
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,112件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by probatista on Sun Mar 16 16:12:59 MST 2014
Indeed, just checked now, I hadn't noticed Table 2 distinguishing which issues applies to which version.
Thanks for the info!
0 件の賞賛
返信

2,112件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Mar 14 20:41:25 MST 2014
Hi Paulo,
Yes, the  issue has been fixed in RevA version onward. Please see errata link below.
http://www.nxp.com/documents/errata_sheet/ES_LPC176X.pdf
0 件の賞賛
返信

2,112件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfb on Fri Mar 14 16:27:47 MST 2014

Quote: probatista
Since this issue is said to affect only revisions "Rev A" and "-"


In the errata Dated Sep 2013 this issue is stated only to affect revision "-" which precedes Rev A. I understood that the problem was fixed about three years ago in Rev A.
0 件の賞賛
返信

2,112件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by probatista on Fri Mar 14 04:47:55 MST 2014
I asked NXP using the form on their site about my question 1, just got their answer:


Quote:
There is currently no newer version than revision A.

The 551 designates a packaging option: http://www.nxp.com/documents/other/PackingLetterCodeusedinOrderablePartNumber.pdf

Newer revisions replace older revisions, and are not specifically orderable unless we introduce separete type numbers for them.



Please let us know if this does not resolve your inquiry. Your ticket will remain closed if we do not hear from you.



Best Regards,

The NXP Technical Support Team
NXP Semiconductors



0 件の賞賛
返信