LPC17xx MCI EFSL Example Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC17xx MCI EFSL Example Problem

1,259件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yasinidz on Wed Dec 19 04:53:44 MST 2012
Hi,
I'm trying to run EFSL example(using the latest version) on my board. When I tried to read .txt files everything seems ok. But writing part is not working correctly. When i changed file_fwrite(...,'a'); 'a' to 'w' i'm expecting that it must work fine. Because File_w.txt and File_r.txt is in the root directory. 
When i try to add my own code to it i still faced problems while writing  to .txt files. it says ok "x bytes succesfully wroten" but when i looked at .txt file, nothing has been changed. is there any one faced with this problem?
ラベル(1)
0 件の賞賛
返信
1 返信

1,246件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Lien.Nguyen on Wed Dec 19 20:51:28 MST 2012
Hi,
Did you get the latest version from the link http://sw.lpcware.com/?p=lpc177x_8x.git&a=summary. I ran the example and it still works.

Best Regards,
Lien
0 件の賞賛
返信