LPC1788 lcd controller configuration:How to configure LCD_VRAM_BASE_ADDR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788 lcd controller configuration:How to configure LCD_VRAM_BASE_ADDR

2,097件の閲覧回数
Mrzhong
Contributor I

Hi,

      In the project,  LPC1788 use external SDRAM as framebuffer to drive TFT-LCD(320 x 240)。In the routines(LCD) ,there is a code snippet description:

      #define LCD_VRAM_BASE_ADDR ((unsigned long)SDRAM_BASE + 0x00010000)

       // Frame Base Address doubleword aligned
      LPC_LCD->UPBASE = LCD_VRAM_BASE_ADDR & ~7UL ;
      LPC_LCD->LPBASE = LCD_VRAM_BASE_ADDR & ~7UL ;

      Now I have a confusion about the address setting,why address offset is 0x00010000。What is the consideration of this offset setting?

0 件の賞賛
返信
2 返答(返信)

2,082件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Mrzhong,

Could you specify what project you are using? Are you using an LPCOpen example code? Where did you find this code snippet?

Most likely, this is to offset the address into the correct section of the memory map. Please look into section 2.1 of the User Manual for more information on peripheral addressing:

https://www.nxp.com/webapp/Download?colCode=UM10470

 

BR,

Edwin.

0 件の賞賛
返信

2,072件の閲覧回数
Mrzhong
Contributor I

Hi,

        In LPCOpen example code, I didn't find example about LCD.In the website:https://www.embeddedartists.com/products/lpc1788-developers-kit/there is an example s_display_truly_lcd_32 in lpc1788_samples_150612 software resources.

         In this example code,there is a code snippet description in sdram.h 

         #define SDRAM_SPEED SDRAM_SPEED_60

         #define SDRAM_CONFIG_32BIT
         #define SDRAM_SIZE 0x2000000

         #define SDRAM_BASE 0xA0000000    /*CS0*/    

      Chapter 2: LPC178x/7x Memory map,  0xA000 0000 - 0xAFFF FFFF is  Dynamic memory chip select 0 (up to 256MB).

       We use  RGB888 color depth and put framebuffer in external SDRAM。In the main.c , there is a code snippet description  about  framebuffer:

         #define DISPLAY_WIDTH 240
         #define DISPLAY_HEIGHT 320

         ...

        int32_t framebuf = (int32_t)(SDRAM_BASE+0x10000);
       sdram_init();
       memset((void*)(framebuf), 0x00, 240*320*2);
       /*dev_lcd = */truly_lcd_open(framebuf);
      fblog = (COLOR_T*)framebuf;

      Combined with other example code related LCD ,  the framebuffer  was always setted  equal  to SDRAM_BASE  plus  0x10000  no mater what  the resolution of LCD  is, such as 240x320, 480 x 272. My confusion is why not use SDRAM_BASE  as the beginning address of frambuffer? In this scenario, the offset   0x10000 is a fixed value or a random value?

     

 

 

0 件の賞賛
返信