LPC1788 and SDRAM 512Mbit structured as 4 Meg x 32 bits x 4 banks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788 and SDRAM 512Mbit structured as 4 Meg x 32 bits x 4 banks

13,048件の閲覧回数
aut
Contributor I

I'm using an external SDRAM connected to the LPC1788FDB208 microcontroller. As SDRAM I chose (and unfortunately already bought many pieces) the IS42S32160F-7TLI model ( http://www.issi.com/WW/pdf/42-45R-S-32160F.pdf  ). This model is a 512Mbit SDRAM structured as 4Mx32x4 (4 Meg x 32 bits x 4 banks). Reading the LPC17xx user manual I seem to understand that the LPC17_xx family doesn't support the 512Mbit SDRAM structured as 4M x 32 x 4 banks, is this correct? Did I well understand? If yes (the LPC17_xx family doesn't support the 4M x 32 x 4 banks configuration) is it possible to use my 512 Mbit SDRAM as a 256 Mbit? If yes, how do I have to configure the DINAMICCONFIG0 register? 

Many thanks 

ラベル(1)
0 件の賞賛
返信
13 返答(返信)

12,733件の閲覧回数
aut
Contributor I

Hi jeremyzhou, many thanks fot the clarification!!

Now I have to understand why the routine

EMC_FUNC_CODE EMC_DynMemConfigAM(uint32_t index,
                                 uint8_t addr_bus_width,
                                 uint8_t addr_map,
                                 uint8_t data_bus_width,
                                 uint16_t chip_size)    

finds "add_mapped_p1=17" instead of "add_mapped_p1=13"

Regards

0 件の賞賛
返信

12,733件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Nico Aprile,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Please follow the below guide to implement it.

pastedImage_4.png

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

12,733件の閲覧回数
aut
Contributor I

Hi jeremyzhou,

many thanks for your support.

Sorry, but I don't understand what setting I have to choose. The table 134 of the attached file shows the possible configuration, can you tell me what I have to choose? From the hardware point of view, is there any modify to do?

Regards

 

0 件の賞賛
返信

12,733件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi

Thanks for your reply.
1) The table 134 of the attached file shows the possible configuration, can you tell me what I have to choose?
-- Please check the Fig 1.

pastedImage_1.png

Fig 1


2) From the hardware point of view, is there any modifications to do?
-- No, just like you connect a 32-bit SDRAM(as the Fig2 shows).

pastedImage_6.png

Fig 2

Hope this is clear.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

12,733件の閲覧回数
aut
Contributor I

Hi jeremyzhou‌,

I followed your indication but the new 512 Mbit memory doesn't work fine. Is there any setting I have to do?

The memory work fine (it seems to me) only if the address mapping bits 14:7 are as follow

bit 14=1

bit 13=0

bit 12=1

bit 11=0

bit 10=1

bit 9=0

bit 8=1

bit 7=0   

but in this case the memory works as a 128 Mbit (4Mx32) 

Have you any suggestion? 

Many thanks.

0 件の賞賛
返信

12,733件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Nico Aprile,

Thank you for your reply.
Whether you tell me What the new 512Mb SDRAM you use.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

12,731件の閲覧回数
aut
Contributor I

Hi, jeremyzhou,

old SDRAM (128 Mb) is the IS42S32400F model (http://www.issi.com/WW/pdf/42-45S32400F.pdf)

new SDRAM (512 Mb) is the IS42R32160F model (http://www.issi.com/WW/pdf/42-45R-S-32160F.pdf)

Below the new SDRAM connections 

pastedImage_1.png

Attached you can find my SDRAM configuration and test code

Many thanks

Regards

0 件の賞賛
返信

12,731件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Thanks for your reply.
1. It seems a bit weird that the SDRAM would work well after setting the addressing map as the Fig1 illustrates, it is definitely inconsistent with its datasheet. So I have no idea now.

pastedImage_1.png

Fig 1

2. I've attached an SDRAM demo, please use it as the template demo code and run it for testing.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a

0 件の賞賛
返信

12,731件の閲覧回数
aut
Contributor I

Hi jeremyzhou‌,

Now the SDRAM seems to work fine. I used the routines you sent me but I had to change something. I had to force the "add_mapped_p1" value. The routine modified is the following:

EMC_FUNC_CODE EMC_DynMemConfigAM(uint32_t index,
                                 uint8_t addr_bus_width,
                                 uint8_t addr_map,
                                 uint8_t data_bus_width,
                                 uint16_t chip_size)    

  {
    const int chip_max_size = 512; // 512Mb
    uint8_t data_bus_max_size = 0;
    uint32_t add_mapped_p1 = 0x00, add_mapped_p2 = 0x00, add_mapped_p3 = 0x00;
    uint32_t tmp = 16, i = 0, j = 0;

    /* Get part 3 of address map */
    switch(addr_bus_width)
      {
        case 16:
          add_mapped_p3 = 0;
          data_bus_max_size = 16;
        break;
        case 32:
          add_mapped_p3 = 1;
          data_bus_max_size = 32;
          break;
        default:
          return EMC_FUNC_INVALID_PARAM;
      }

    /* Get part 2 of address map */
    add_mapped_p2 = EMC_DYNAMIC_CFG_ADD_MAP_P2(addr_map);


    /* Get part 1 of address map */
    if(chip_size == 16)
      {
        if (data_bus_width == 8) add_mapped_p1 = 0;
        else if(data_bus_width == 16) add_mapped_p1 = 1;
        else return EMC_FUNC_INVALID_PARAM;
      }
    else
      {
        while(1)
          {
            i++;
            tmp = 16*(0x01 << (i+1));
            if(tmp == chip_size)
              {
                for(j = 0; (8<<j)<=data_bus_max_size;j++)
                  {
                    if((8<<j) == data_bus_width) break;
                  }
                if( (8<<j) > data_bus_max_size) return EMC_FUNC_INVALID_PARAM;

                add_mapped_p1 = (i<<2) + j;
                break;
              }
            if(tmp >= chip_max_size)
              {
                return EMC_FUNC_INVALID_PARAM;
              }
          }
      }

    //SDRAM ISSI da 512 Mbit model IS42S32160F_7TLI 16Mx32 (4M x 32 bit x 4 bank)
    add_mapped_p1=13; //


    switch(index)
      {
        case 0:
          LPC_EMC->DynamicConfig0 &= ~EMC_DYNAMIC_CFG_ADD_MAP_P1_MASK;
          LPC_EMC->DynamicConfig0 |= EMC_DYNAMIC_CFG_ADD_MAP_P1(add_mapped_p1);
          LPC_EMC->DynamicConfig0 &= ~EMC_DYNAMIC_CFG_ADD_MAP_P2_MASK;
          LPC_EMC->DynamicConfig0 |= EMC_DYNAMIC_CFG_ADD_MAP_P2(add_mapped_p2);
          LPC_EMC->DynamicConfig0 &= ~EMC_DYNAMIC_CFG_ADD_MAP_P3_MASK;
          LPC_EMC->DynamicConfig0 |= EMC_DYNAMIC_CFG_ADD_MAP_P3(add_mapped_p3);
        break;
        case 1:
          LPC_EMC->DynamicConfig1 &= ~EMC_DYNAMIC_CFG_ADD_MAP_P1_MASK;
          LPC_EMC->DynamicConfig1 |= EMC_DYNAMIC_CFG_ADD_MAP_P1(add_mapped_p1);
          LPC_EMC->DynamicConfig1 &= ~EMC_DYNAMIC_CFG_ADD_MAP_P2_MASK;
          LPC_EMC->DynamicConfig1 |= EMC_DYNAMIC_CFG_ADD_MAP_P2(add_mapped_p2);
          LPC_EMC->DynamicConfig1 &= ~EMC_DYNAMIC_CFG_ADD_MAP_P3_MASK;
          LPC_EMC->DynamicConfig1 |= EMC_DYNAMIC_CFG_ADD_MAP_P3(add_mapped_p3);
        break;
        case 2:
          LPC_EMC->DynamicConfig2 &= ~EMC_DYNAMIC_CFG_ADD_MAP_P1_MASK;
          LPC_EMC->DynamicConfig2 |= EMC_DYNAMIC_CFG_ADD_MAP_P1(add_mapped_p1);
          LPC_EMC->DynamicConfig2 &= ~EMC_DYNAMIC_CFG_ADD_MAP_P2_MASK;
          LPC_EMC->DynamicConfig2 |= EMC_DYNAMIC_CFG_ADD_MAP_P2( add_mapped_p2);
          LPC_EMC->DynamicConfig2 &= ~EMC_DYNAMIC_CFG_ADD_MAP_P3_MASK;
          LPC_EMC->DynamicConfig2 |= EMC_DYNAMIC_CFG_ADD_MAP_P3(add_mapped_p3);
        break;
        case 3:
          LPC_EMC->DynamicConfig3 &= ~EMC_DYNAMIC_CFG_ADD_MAP_P1_MASK;
          LPC_EMC->DynamicConfig3 |= EMC_DYNAMIC_CFG_ADD_MAP_P1(add_mapped_p1);
          LPC_EMC->DynamicConfig3 &= ~EMC_DYNAMIC_CFG_ADD_MAP_P2_MASK;
          LPC_EMC->DynamicConfig3 |= EMC_DYNAMIC_CFG_ADD_MAP_P2(add_mapped_p2);
          LPC_EMC->DynamicConfig3 &= ~EMC_DYNAMIC_CFG_ADD_MAP_P3_MASK;
          LPC_EMC->DynamicConfig3 |= EMC_DYNAMIC_CFG_ADD_MAP_P3(add_mapped_p3);
        break;
        default:
        return EMC_FUNC_INVALID_PARAM;
      }
    return EMC_FUNC_OK;
  }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

The original routine calculated:

add_mapped_p1=17
add_mapped_p2=0
add_mapped_p3=1‍‍‍‍‍‍

but using add_mapped_p1=17 the SDRAM doesn't work fine. I have to force

add_mapped_p1=13

In this way  the SDRAM works fine. Why your routine doesn't calcule the right add_mapped_p1 value? 

The SDRAM timing I used are the following:

//SDRAM ISSI da 512 Mbit model IS42S32160F_7TLI 16Mx32 (4M x 32 bit x 4 bank)
config.ChipSize             = 512;                      // 512 Mbit total 
config.AddrBusWidth         = 32;                       // 32 bit address bus
config.AddrMap              = EMC_ADD_MAP_ROW_BANK_COL;
config.CSn                  = 0;
config.DataWidth            = 16;                       
config.TotalSize            = 536870912;

config.CASLatency           = 2;                        // CAS
config.RASLatency           = 1;                        // RAS
config.Active2ActivePeriod  = 10;                       // tRC
config.ActiveBankLatency    = 2;                        // tRRD
config.AutoRefrehPeriod     = 10;                       // tRFC/tRC
config.DataIn2ActiveTime    = 5;                        // tDAL, or tAPW
config.DataOut2ActiveTime   = 5;                        // tAPR
config.WriteRecoveryTime    = 2;                        // tWR, tDPL, tRWL, or tRDL
config.ExitSelfRefreshTime  = EMC_NS2CLK(70);           // tXSR
config.LoadModeReg2Active   = 2;                        // tMRD
config.PrechargeCmdPeriod   = 3;                        // tRP
config.ReadConfig           = 1;                        
config.RefreshTime          = EMC_SDRAM_REFRESH(64);
config.Active2PreChargeTime = 7;                        // tRAS
config.SeftRefreshExitTime  = EMC_NS2CLK(70);
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

The configuration 

add_mapped_p1=13
add_mapped_p2=0
add_mapped_p3=1‍‍‍‍‍‍

correspond to 

pastedImage_1.png

Your previous suggestion was 

pastedImage_1.png

I am a little bit confuse.. Smiley Happy. Can you explain me?

Many thanks

Regards 

0 件の賞賛
返信

12,731件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Nico Aprile,

According to the below statement (Fig 1), the Fig 2 is correct, so I made a mistake before.

Hope this is clear.

pastedImage_4.png

Fig 1

pastedImage_1.png

Fig 2


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

12,731件の閲覧回数
aut
Contributor I

Hi jeremyzhou,

many, many thanks!

Your indication is:

pastedImage_3.png

Why not the following?:

pastedImage_4.png

In other words, what's the bit 12 function

Have a nice day.

Regards

0 件の賞賛
返信

12,731件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Nico Aprile,

Thanks for your reply.
Actually, both are available.
However, It's the 16-bit external bus high-performance address mapping when the bit 12 is 0.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

12,731件の閲覧回数
aut
Contributor I

jeremyzhou,  I thank you very much!

Regards.

0 件の賞賛
返信