LPC1788 USB HID for Mac OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788 USB HID for Mac OS

2,151 Views
parkjungho
Contributor I

Hello, all!

I am using LPC1788FBD208. I am testing HID on NXPUSBLIB(LPCOpen).

In case of Windows, I confirmed that the HID driver is installed automatically.

However, the driver is not automatically installed on the Mac PC.

Does Mac OS need to install drivers separately to control general HID?

I do not know much about Mac OS.

How do I enable LPC HID on Mac OS?

Have a nice day. Thank you.

Labels (3)
0 Kudos
Reply
2 Replies

1,877 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the below link and let me know if this helps.

LPC USB Serial I/O Library | www.LPCware.com 

https://community.nxp.com/thread/388960 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,877 Views
parkjungho
Contributor I

Hi, Sol.

Thank you for the reply.

I'll check the related links to see if they can help me with my issue.

Thank you.

0 Kudos
Reply