LPC1788 USB HID for Mac OS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 USB HID for Mac OS

2,194 次查看
parkjungho
Contributor I

Hello, all!

I am using LPC1788FBD208. I am testing HID on NXPUSBLIB(LPCOpen).

In case of Windows, I confirmed that the HID driver is installed automatically.

However, the driver is not automatically installed on the Mac PC.

Does Mac OS need to install drivers separately to control general HID?

I do not know much about Mac OS.

How do I enable LPC HID on Mac OS?

Have a nice day. Thank you.

标签 (3)
0 项奖励
回复
2 回复数

1,920 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please check the below link and let me know if this helps.

LPC USB Serial I/O Library | www.LPCware.com 

https://community.nxp.com/thread/388960 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,920 次查看
parkjungho
Contributor I

Hi, Sol.

Thank you for the reply.

I'll check the related links to see if they can help me with my issue.

Thank you.

0 项奖励
回复