LPC1788 RTC's General purpose registers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788 RTC's General purpose registers

1,599件の閲覧回数
lihai
Contributor II

Dear All,

     I have a question about LPC1788 RTC's General purpose registers 0-4,   I write 1 to General purpose registers 0 , then power off(without battery powered) , General purpose registers 0 value changed to 0 after power on. 

     the user manual said : These registers can be used to store import information when the main power supply is off .  It seems that General purpose registers can not store information without main power supply & battery power supply?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,450件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

The RTC block includes 20 bytes of battery-powered backup registers, allowing system status to be stored when the rest of the chip is powered off. Battery power can be supplied from a standard 3 V Lithium button cell. 

I hope this clarifies.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信