LPCScrypt load spi flash data to binary file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCScrypt load spi flash data to binary file

1,565 Views
kensu
Contributor V

Hi,

Can I use LPCScrypt to read back the SPIFI flash data to binary file?

I check the document, it only have SPIFIRead command, but it only read the sum?

pastedImage_1.png

Thanks

Ken

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,455 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ken Su,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Can I use LPCScrypt to read back the SPIFI flash data to a binary file?
-- I'm afraid not.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply