LPC1788 RTC's General purpose registers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 RTC's General purpose registers

1,712 次查看
lihai
Contributor II

Dear All,

     I have a question about LPC1788 RTC's General purpose registers 0-4,   I write 1 to General purpose registers 0 , then power off(without battery powered) , General purpose registers 0 value changed to 0 after power on. 

     the user manual said : These registers can be used to store import information when the main power supply is off .  It seems that General purpose registers can not store information without main power supply & battery power supply?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,563 次查看
soledad
NXP Employee
NXP Employee

Hi,

The RTC block includes 20 bytes of battery-powered backup registers, allowing system status to be stored when the rest of the chip is powered off. Battery power can be supplied from a standard 3 V Lithium button cell. 

I hope this clarifies.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复