LPC1788 GPIO High Impedance state

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788 GPIO High Impedance state

2,338件の閲覧回数
anujtanksali
Contributor II

Hi,

I am using LPC 1788. I want to set one gpio in high impedance state.

I have configured the pin as input and set open drain enable. Is this the correct way of setting the pin in high impedance state

Thanks

Regards,

Anuj

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,899件の閲覧回数
anujtanksali
Contributor II

Hi,

Thanks a lot for your timely response.

Regards,

Anuj

0 件の賞賛
返信

1,899件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi Anuj,

You are correct, set the GPIO pin to be an input and open drain with no pull resistor if you want it to have a high impedance.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信