LPC1788 GPIO High Impedance state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788 GPIO High Impedance state

2,363 Views
anujtanksali
Contributor II

Hi,

I am using LPC 1788. I want to set one gpio in high impedance state.

I have configured the pin as input and set open drain enable. Is this the correct way of setting the pin in high impedance state

Thanks

Regards,

Anuj

Labels (1)
0 Kudos
Reply
2 Replies

1,924 Views
anujtanksali
Contributor II

Hi,

Thanks a lot for your timely response.

Regards,

Anuj

0 Kudos
Reply

1,924 Views
soledad
NXP Employee
NXP Employee

Hi Anuj,

You are correct, set the GPIO pin to be an input and open drain with no pull resistor if you want it to have a high impedance.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply