LPC1778FET208 GPIO Current Output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1778FET208 GPIO Current Output

Jump to solution
2,673 Views
VMS
Contributor I

Hi,

How much current we can draw from GPIO port pins in LPC1778FET208.

0 Kudos
Reply
1 Solution
2,649 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Venkatesh,

The source current means the GPIO outputting current when the GPIO pin outputs logic high, the higher the source current is, the higher voltage drop is. The 4mA current means that we can guarantee that the voltage drop is less than 400mV when the source current is 4mA.

I copy the Fig from the data sheet of LPC177x. which can be downloaded from the link:

https://www.nxp.com.cn/docs/en/data-sheet/LPC178X_7X.pdf

 

The sink current is the current the pin draws when the GPIO pin outputs LOW logic. The higher the sink current is, the higher the GPIO pin voltage is. The 4mA sink current means that we can guarantee the pin voltage rising is less than 400mV when the pin draws 4mA current.

 

Hope it can help you

 

xiangjun_rong_0-1603334966427.pngxiangjun_rong_0-1603334966427.png

 

 

View solution in original post

0 Kudos
Reply
3 Replies
2,663 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Friend,

Pls refer to Table 13. Static characteristics … in data sheet of LPC177x, both the source/sink current is 4mA.

 
 

source_sinkCurrent.pngsource_sinkCurrent.png

Hope it can help you

BR

XiangJun Rong

 
 

 

0 Kudos
Reply
2,658 Views
VMS
Contributor I

Hi Xiangjun,

Thanks for your kind reply, in datasheet it is mentioned only minimum current this means we can able to draw 4mA maximum.

 

0 Kudos
Reply
2,650 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Venkatesh,

The source current means the GPIO outputting current when the GPIO pin outputs logic high, the higher the source current is, the higher voltage drop is. The 4mA current means that we can guarantee that the voltage drop is less than 400mV when the source current is 4mA.

I copy the Fig from the data sheet of LPC177x. which can be downloaded from the link:

https://www.nxp.com.cn/docs/en/data-sheet/LPC178X_7X.pdf

 

The sink current is the current the pin draws when the GPIO pin outputs LOW logic. The higher the sink current is, the higher the GPIO pin voltage is. The 4mA sink current means that we can guarantee the pin voltage rising is less than 400mV when the pin draws 4mA current.

 

Hope it can help you

 

xiangjun_rong_0-1603334966427.pngxiangjun_rong_0-1603334966427.png

 

 

0 Kudos
Reply