LPC1778 iap entry 0x1FFF1FF0 data error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1778 iap entry 0x1FFF1FF0 data error

2,368 Views
haopengtang
Contributor I

我创建了一个在ram中运行的代码准备测试iap功能。

1、如果我使用jlink工具先片擦除ROM。这是为了确保内部flash都是0xff。然后我在ram中进行仿真发现IAP的入口地址0x1FFF_1FF0处的数据都是0x0000_0000. 这时执行IAP进行flash操作就会出错。

2、如果我先下载一个比如闪灯的代码到flash 0地址开始处。在进行ram仿真,发现IAP的入口地址数据变成了0xbb1af7ff.这时就能使用iap进行flash操作。

请问是什么原因导致0x1fff1fff0 地址的数据出现错误

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,924 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

我手头没有LPC1778的板子,所以用LPC1788的板子做了个测试。

使用J-Link Commander工具完全擦除LPC1788芯片后,读取0x1FFF1FF0地址的值如下:

pastedImage_0.png

如果你手头也有J-Link工具,也可以测试一下(输入下列命令):

usb

device ? (选择NXP LPC1778)

erase all

mem32 0x1fff1ff0 0x10

Segger J-Link Commander 软件可以从这里下载。


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply