LPC1778 erase eeprom

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1778 erase eeprom

2,302 Views
Navium
Contributor I

Hello everyone.

I have connection with LPC1778 with Flash Magic in ISP

Is there is any firmware that i can flash which

- erases eeprom or write zeroes in it and then

- goes back to ISP mode

Thank you for answers.

0 Kudos
Reply
6 Replies

2,213 Views
Navium
Contributor I

Okay. Lets simplify question.

How to erase eeprom?

Is there is any solution?

0 Kudos
Reply

2,117 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Navium 

There is EEPROM demo under "periph_eeprom" LPCopen. You can refer it. 

Alice_Yang_0-1733883147968.pngAlice_Yang_0-1733883147968.png

Thanks.

BR

Alice

0 Kudos
Reply

2,258 Views
Navium
Contributor I

Yes i know that i can not program eeprom with FlashMagic.

Can i program on-chip memory to erase eeprom?

 

0 Kudos
Reply

2,277 Views
Navium
Contributor I

Yes i know 

Can i program chip memory to erase eeprom?

0 Kudos
Reply

2,278 Views
Navium
Contributor I

Yes, i know that i can not erase eeprom in LPC1778 with FlashMagic

But i can flash firmware that will erase eeprom.

Is there is any firmware that can do it?

0 Kudos
Reply

2,285 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Navium 

For LPC1778, ISP is programming or reprogramming the on-chip flash memory, using the boot loader software and UART0. Can not program EEPROM.

BR

Alice

0 Kudos
Reply