LPC1769 QEI example in LPCOpen?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1769 QEI example in LPCOpen?

ソリューションへジャンプ
4,475件の閲覧回数
MAPC
Senior Contributor I

Hello,

Does anybody have any example code for LPC1769 Quadrature Encoder Interface? I haven't found it in LPC1769 LPCOpen package.

Thanks!

Marco Coelho

DFAE - Siletec Eletronica

ラベル(2)
0 件の賞賛
返信
1 解決策
3,817件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Marco Aurelio P. Coelho,

Thank you for your interest in NXP Semiconductor products and 

the opportunity to serve you.

Please checking the attachment.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,818件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Marco Aurelio P. Coelho,

Thank you for your interest in NXP Semiconductor products and 

the opportunity to serve you.

Please checking the attachment.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,817件の閲覧回数
MAPC
Senior Contributor I

Thank you very much, Jeremy Zhou

Do you have a document explaining in more detail how this example works?

Your example runs in KEIL. What should we do to port this project to MCUXpresso?

Best regards,

Marco Coelho

0 件の賞賛
返信
3,817件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Marco Aurelio P. Coelho,

Thanks for your reply.

The QEI demo not only can run in the KEIL but also can run in the IAR, however you should manually porting if you prefer the MCUXpresso.

The attached file has introduced the QEI demo in details and I think you can get the overview of the demo after reading it.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,817件の閲覧回数
MAPC
Senior Contributor I

Hi jeremyzhou

I just ported the example that you sent me to MCUXpresso. It is compiling perfectly. I don't know if it is running in a LPC1769, because I don't have a kit with this MCU here. But, it is supposed to be working.

Anyway, thank you very much for your help! Surely, it will be very helpful for the customer!

Best regards,

Marco Coelho

DFAE - Siletec Eletronica

0 件の賞賛
返信
3,817件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Marco Aurelio P. Coelho,

Thanks for your reply.

The QEI demo is available to LPC175x/6x series, definitely it includes the LPC1769.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,817件の閲覧回数
MAPC
Senior Contributor I

Hi jeremyzhou

The LPCOpen drivers from the example that you sent me are completely different from those which are in MCUXpresso LPCOPen.

Probably it won't be possible to reuse code and will be necessary to write a new project. If there was a demo code, it would be very helpful for us, but if there isn't, no problem...

Marco Coelho

DFAE - Siletec Eletronica

0 件の賞賛
返信