LPC1769 I2C Help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 I2C Help

1,032 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by odel1830 on Thu Feb 27 13:53:22 MST 2014
I am writing code to interact with a temp sensor, I am having some trouble with it.

I am looking at the LPC17xx User manual, Chpt 19.10.5.3. I am looking at State: 0x08 and I am trying to transmit a start condition. State 0x08 is below. My question is about parts 4, 5, and 6. I don't understand how to set those up. Can anyone help?


State: 0x08

A START condition has been transmitted. The Slave Address + R/W bit will now be
transmitted.

1. Write Slave Address with R/W bit to I2DAT.
2. Write 0x04 to I2CONSET to set the AA bit.
3. Write 0x08 to I2CONCLR to clear the SI flag.
4. Set up Master Transmit mode data buffer.
5. Set up Master Receive mode data buffer.
6. Initialize Master data counter.
7. Exit
Labels (1)
0 Kudos
Reply
0 Replies