LPC1769 Debug problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 Debug problem

2,033 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by db123 on Sat Oct 12 07:17:43 MST 2013
Hello All,

Recently i got LPC1769 LPCXpresso board. And i'm unable to flash the example program into the target.
The build was success and when i click "Debug" the error dialog box prompts.
Please have a look at error prompt attached below.

If i click "Proceed" button then another prompt comes with message "Program file does not exist".
The file name it is looking is "LPCX176x_cmsis2_systick.axf".

Kindly help to resolve this error.

thanks.
Labels (1)
0 Kudos
Reply
1 Reply

1,962 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tha on Sat Oct 12 23:11:07 MST 2013
In the LPCXpresso IDE, you need to build all related projects in addition to your main project.  From your error, it seems like you are using the CMSIS file, so this mean you have to build the CMSIS project first, then click on debug for your main project.
0 Kudos
Reply