LPC1769 DAC - voltage DAC output trouble

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 DAC - voltage DAC output trouble

2,426 Views
jakubpapuga-sza
Contributor II

Hi,

I have LPCXpresso LPC1769 Rev.D board and I need to use DAC to controll some external device.

I unsoldered L1 BK1608HS220-T from LPCXpresso LPC1769 and I connected directly my reference voltage source - REF193.

I have some troubles with LPC1769 DAC. There is no output voltage as should be.

Below is a table with results (DAC Sens = 2,9297 mV/sa = 3000 mV/1024 sa):

0 sa - 17,7 mV (should be 0 V)

5 sa - 32,5 mV (should be 14,6 mV)

10 sa - 46,7 mV (should be 29,3 mV

20 sa - 75,8 mV (should be 58,6 mV)

30 sa - 104,6 mV (should be 87,9 mV)

40 sa - 134,5 mV (should be 117,2 mV)

50 sa - 163,5 mV (should be 146,5 mV)

multimeter BRYMEN BM811A

There is a chart in attachement with my DAC voltage output values...

There is some nonlinear bias/offset.

What is wrong? Do I need something else for my DAC?

Labels (2)
0 Kudos
Reply
0 Replies