LPC1768 write to flash without a erasing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1768 write to flash without a erasing

8,224件の閲覧回数
bjoern_harre
Contributor I

I have reserved one flash page for saving an operating hours counter. There is an array of 32 entries in RAM of "unsinged long". This array is also filled with "0xFFFFFFFF". Every hour the index for the array is incremented by "1". After reaching the last entry, the index is set to "0" and the flash page will be erased. On the first run, the reserved flash page is cleared (every entry is 0xFFFFFFFF) and the array is also filled with 0xFFFFFFFF. After every hour, the complete array is copied into flash, without erasing. This shall work, because writing the same values or wriring the new last updated array entry value shall work. Sometimes this stategy fails and the stored data in flash is not the same as in the array. Why is it so? If I erase the flash page before write the new content of array, it works. But I don't want to erase the flash page every hour. My stategy is to ease it every 32 hours to save writing cycles.

Screenshot of memory content:

-sOPHours stored in RAM

-csOPHours stored in FLASH

The last new entry was 1077. During write RAM into FLASH, the entry of index 20 was set to an invalid value, Why?

 

0 件の賞賛
返信
9 返答(返信)

8,149件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello bjoern_harre,

It is better erase before every write flash.

 

BR

Alice

0 件の賞賛
返信

8,198件の閲覧回数
bjoern_harre
Contributor I

and this is with erasing:

 

//prepare for sector erasing
ulCommand[0]=PREPARE_FLASH2WRITE;
ulCommand[1]=ucGetSector_Number((unsigned long)ulDest);
ulCommand[2]=ucGetSector_Number((unsigned long)(ulDest)+ulSize-1);
ulCommand[3]=SystemCoreClock / 1000;
iap_entry((unsigned int*)&ulCommand[0],(unsigned int*)&ulResult[0]);
//maybe test for errors
if (ulResult[0] != 0)
{
taskEXIT_CRITICAL();
return;
}
//erase sectors
ulCommand[0]=ERASESECTORS;
iap_entry((unsigned int*)&ulCommand[0],(unsigned int*)&ulResult[0]);
//maybe test for errors
if (ulResult[0] != 0)
{
taskEXIT_CRITICAL();
return;
}

//prepare for sector writing
ulCommand[0]=PREPARE_FLASH2WRITE;
ulCommand[1]=ucGetSector_Number((unsigned long)pDest);
ulCommand[2]=ucGetSector_Number((unsigned long)pDest+sizeof(ucBuffer)-1);
iap_entry((unsigned int*)&ulCommand[0],(unsigned int*)&ulResult[0]);
//maybe test for errors
if (ulResult[0] != 0)
{
taskEXIT_CRITICAL();
return;
}
ulCommand[0]=COPYRAM2FLASH;
ulCommand[1]=(unsigned long)pDest;
ulCommand[2]=(unsigned long)&ucBuffer[0];
ulCommand[3]= sizeof(ucBuffer)/4;
ulCommand[4]=SystemCoreClock / 1000;
iap_entry((unsigned int*)&ulCommand[0],(unsigned int*)&ulResult[0]);
//maybe test for errors
if (ulResult[0] != 0)
{
taskEXIT_CRITICAL();
return;
}

 

 

0 件の賞賛
返信

8,209件の閲覧回数
bjoern_harre
Contributor I

Here it is:

 

//prepare for sector writing
ulCommand[0]=PREPARE_FLASH2WRITE;
ulCommand[1]=ucGetSector_Number((unsigned long)pDest);
ulCommand[2]=ucGetSector_Number((unsigned long)pDest+sizeof(ucBuffer)-1);
iap_entry((unsigned int*)&ulCommand[0],(unsigned int*)&ulResult[0]);
//maybe test for errors
if (ulResult[0] != 0)
{
taskEXIT_CRITICAL();
return;
}
ulCommand[0]=COPYRAM2FLASH;
ulCommand[1]=(unsigned long)pDest;
ulCommand[2]=(unsigned long)&ucBuffer[0];
ulCommand[3]= sizeof(ucBuffer)/4;
ulCommand[4]=SystemCoreClock / 1000;
iap_entry((unsigned int*)&ulCommand[0],(unsigned int*)&ulResult[0]);
//maybe test for errors
if (ulResult[0] != 0)
{
taskEXIT_CRITICAL();
return;
}

 

ulResult[0] is always "0". SystemCoreClock is 100MHz.

0 件の賞賛
返信

8,189件の閲覧回数
converse
Senior Contributor V

Some comments.

Have you read section 5.2.2 of the user manual? There is an interesting comment about the flash accelerator maybe returning stale data if not using erase.

have you reserved the top 32 bytes of ram for the flash programmer? 32.3.2.7 in the user manual 

 

0 件の賞賛
返信

8,187件の閲覧回数
bjoern_harre
Contributor I

I am not using the watchdog. Interruptes are disabled during erasing, writing and comparing. There is a reserved memory area of 32 bytes @ 0x10007FE0.

I have made a small statistic:

write accesses:  6539

store invalid data: 1896

 

0 件の賞賛
返信

8,184件の閲覧回数
converse
Senior Contributor V

The 2nd paragraph of 5.2.2 is the interesting bit - not the bit about watchdog. See below

have you verified that you get no errors if you perform the erase first? I.e. check that there is not another issue here.

 

In order to preclude the possibility of stale data being read from the flash memory, the LPC176x/5x flash accelerator buffers are automatically invalidated at the beginning of any flash programming or erase operation. Any subsequent read from a flash address will cause a new fetch to be initiated after the flash operation has completed.

0 件の賞賛
返信

8,155件の閲覧回数
bjoern_harre
Contributor I

Do you know any other work a round? Or shall I increase the flash wait states?

0 件の賞賛
返信

8,181件の閲覧回数
bjoern_harre
Contributor I

Every "result" after erasing or writing is "0".

Do you mean this at 5.2.2:"In order to preclude the possibility of stale data being read from the flash memory, the LPC176x/5x flash accelerator buffers are automatically invalidated at the beginning of any flash programming or erase operation. Any subsequent read from a flash address will cause a new fetch to be initiated after the flash operation has completed."

The content of flash is always invalid, after many readings. The case of invalid stored data is realy random.

0 件の賞賛
返信

8,213件の閲覧回数
converse
Senior Contributor V

Could you share your code for programming flash (with and without erase). You may be missing a step.

0 件の賞賛
返信