LPC1768 MCPWM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1768 MCPWM

3,752 次查看
mallikarjunared
Contributor III

Hey Guys,

       I wanted to use Motor Control PWM as Normal PWM since my Normal PWM was used for other purpose.

I am using LPCOpen(where as MCPWM is  not available) library, Can some one help me on this.

Thanks & Regards,

Mallikarjuna Reddy

标签 (2)
0 项奖励
回复
2 回复数

2,419 次查看
mahdikan
Contributor I

hi friends i cant find this link please tell me the new link thanks

cmsis standard peripheral firmware driver library

0 项奖励
回复

3,316 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Mallikarjuna Reddy,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
To provide the fastest possible support I want to point you to refer to
the MCPWM demo which is from the LPC175x CMSIS-Compliant Standard Peripheral
Firmware Driver Library whose download link is below:
LPC175x_6x CMSIS-Compliant Standard Peripheral Firmware Driver Library (Keil, IAR, GNU) | www.LPCwar... 

Hope this helps.
Have a great day,
Ping

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复