LPC1768 MCPWM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 MCPWM

3,768 Views
mallikarjunared
Contributor III

Hey Guys,

       I wanted to use Motor Control PWM as Normal PWM since my Normal PWM was used for other purpose.

I am using LPCOpen(where as MCPWM is  not available) library, Can some one help me on this.

Thanks & Regards,

Mallikarjuna Reddy

Labels (2)
0 Kudos
Reply
2 Replies

2,435 Views
mahdikan
Contributor I

hi friends i cant find this link please tell me the new link thanks

cmsis standard peripheral firmware driver library

0 Kudos
Reply

3,332 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Mallikarjuna Reddy,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
To provide the fastest possible support I want to point you to refer to
the MCPWM demo which is from the LPC175x CMSIS-Compliant Standard Peripheral
Firmware Driver Library whose download link is below:
LPC175x_6x CMSIS-Compliant Standard Peripheral Firmware Driver Library (Keil, IAR, GNU) | www.LPCwar... 

Hope this helps.
Have a great day,
Ping

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply