LPC1768 Internal RTC lag 4.5min/hr

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 Internal RTC lag 4.5min/hr

3,296 Views
omkar787898
Contributor II

I am using Internal RTC of LPC1768 but is lagging by 4 & half minutes for 1 hour. Is there any solution to make it accurate or this is the problem of LPC1768 internal RTC?

Labels (5)
0 Kudos
Reply
5 Replies

2,885 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Omkar,

Which silicon revision is your MCU? Please notice that Revision A does not suffer from the RTC.1 erratum. The RTC oscillator is expected to work fine on rev A silicon.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

2,885 Views
omkar787898
Contributor II

Hi,

Thanks for help but Where do i check the which revision i am using, Is

there anything mention on Controller chip?

Thanks & regards,

Omkar Teli.

On Tue, Feb 21, 2017 at 10:53 PM, Carlos_Mendoza <[email protected]>

0 Kudos
Reply

2,885 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Omkar,

 

The LPC176x devices typically have the following top-side marking:

LPC176xxxx

xxxxxxx

xxYYWWR[x]

The last/second to last letter in the third line (field ‘R’) will identify the device revision.


Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

2,885 Views
omkar787898
Contributor II

hi,

there is "LPC1768FBD100

SW1441.1

ZSD1219A"

so it is revision A?

Thanks & regards,

Omkar Teli.

On Thu, Feb 23, 2017 at 5:09 AM, Carlos_Mendoza <[email protected]>

0 Kudos
Reply

2,885 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Omkar,

 

Yes, it is the Rev. A, this revision does not suffer from the RTC.1 erratum. The RTC oscillator is expected to work fine on rev A silicon. Which application are you suing? Have you tried the periph_rtc example that comes with LPCOpen?

LPCOpen Software for LPC17XX|NXP 

 

Best Regards!
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply