How can I write protect sectors of internal flash (LPC1769)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I write protect sectors of internal flash (LPC1769)?

1,576 Views
stenlarsson
Contributor II

I want to protect one or a few 4K internal flash sectors from being erased by the application (on purpose or by mistake). 

Is this possible?

0 Kudos
Reply
2 Replies

1,486 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sten Larsson,

   Unfortunately, the LPC1769 hardware still can't support the flash protection function now.

 

 


Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,486 Views
converse
Senior Contributor V

You cannot protect individual sectors

0 Kudos
Reply