LPC1768 Emwin Font and Image displaying Problem??????

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1768 Emwin Font and Image displaying Problem??????

998 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by AkshayHV on Sat Jan 25 03:40:39 MST 2014
Hello
i am interfacing a 3.2 inch TFT with LPC1768 ,the controller in the display is ILI9341. it is basically a spi interface and i am using a template code of NXP there GUI_FONT_20F_ASCII (which is proportional framed font) working fine for strings like "Hello World!" "www.kiel.com" and "www.segger.com" but for the number which runs from 0 to 9999 at the centre of the display is displaying each number two times for example instead of 0000 it is displaying "00000000" and for "1234" it is displaying "11223344"  other than the GUI_FONT_20F_ASCII font i am not been able to use any other font its is getting scrambled if other fonts are used.

And for displaying image using a GUI_DrawBitmap the image which is converted to BMP using BMPCvt tool by emwin it is getting scrambled  for HIGH color (565) compressed image but it is working for HIGH color (565) i,e without compression.please somebody Help.


Thanks and Regards
Akshay H V
标签 (1)
0 项奖励
回复
0 回复数