LPC1766FBD100,551 alternative

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1766FBD100,551 alternative

3,413件の閲覧回数
RoyJ
Contributor I
Hello, We found the Mcu LPC1766FBD100,551 has been EOL, we use this MCU several years, we want to choose LPC1766FBD100K as a alternative, we want to know if we can use the same firmware as LPC1766FBD100,551? do we need do some modify the firmware?
0 件の賞賛
返信
8 返答(返信)

3,390件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI RoyJ

It's right LPC1766FBD100,551 has been EOL, LPC1766FBD100K is the replacement.

From LPC1766FBD100,551 to LPC1766FBD100K, the only difference is packing format (from tray to brick). inside is the same. that's to say, the chip itself is the same.

Have a nice day

Jun Zhang

0 件の賞賛
返信

3,360件の閲覧回数
RoyJ
Contributor I

Hello Jennie,

Thank you for your kindly reply!

One more question need consult you. Can we use LPC1769FBD100,551 replace LPC1766FBD100,551?

It seems all parameter same except memory size (alternative have larger memory size), so we can switch

to use LPC1769FBD100,551 and no need change firmware, right?

0 件の賞賛
返信

3,345件の閲覧回数
frank_m
Senior Contributor III

>...so we can switch to use LPC1769FBD100,551 and no need change firmware, right?

I think a re-build for the new MCU will be required.

0 件の賞賛
返信

3,340件の閲覧回数
RoyJ
Contributor I

Hello Frank,

So you means I can't use the same Hex file for the alternative? that's will be a problem for me.

0 件の賞賛
返信

3,333件の閲覧回数
frank_m
Senior Contributor III

You will need to try. Perhaps it works, but as other threads here show, there is a good chance it does not.

> that's will be a problem for me.

Could be worse. Perhaps you should have checked to projected lifetime more closely when planning for a project. My company has similar problems with Fujitsu stuff, only there is no similar and compatible replacement.

0 件の賞賛
返信

3,352件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi RoyJ

These two parts are pin to pin replacement. no need change firmware as well.

The main differences are, LPC1769 has higher maximal CPU Frequency(120MHz) and larger memory size(512KB)

Have a nice day,

Jun Zhang

0 件の賞賛
返信

3,339件の閲覧回数
RoyJ
Contributor I

Hello Jennie,

Do we need to re-build the firmware when we change the MCU from LPC1766FBD100,551 to the alternative(LPC1769FBD100,551)?

0 件の賞賛
返信

3,407件の閲覧回数
frank_m
Senior Contributor III

That designations sound very similar, which lead me to believe you could expect an EOL message for this alternative type soon.

But you would need to contact NXP or an official distributor directly - this is not tha type of info given in a public forum like this.

0 件の賞賛
返信