LPC1766FBD100,551 alternative

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1766FBD100,551 alternative

3,407 Views
RoyJ
Contributor I
Hello, We found the Mcu LPC1766FBD100,551 has been EOL, we use this MCU several years, we want to choose LPC1766FBD100K as a alternative, we want to know if we can use the same firmware as LPC1766FBD100,551? do we need do some modify the firmware?
0 Kudos
Reply
8 Replies

3,384 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI RoyJ

It's right LPC1766FBD100,551 has been EOL, LPC1766FBD100K is the replacement.

From LPC1766FBD100,551 to LPC1766FBD100K, the only difference is packing format (from tray to brick). inside is the same. that's to say, the chip itself is the same.

Have a nice day

Jun Zhang

0 Kudos
Reply

3,354 Views
RoyJ
Contributor I

Hello Jennie,

Thank you for your kindly reply!

One more question need consult you. Can we use LPC1769FBD100,551 replace LPC1766FBD100,551?

It seems all parameter same except memory size (alternative have larger memory size), so we can switch

to use LPC1769FBD100,551 and no need change firmware, right?

0 Kudos
Reply

3,339 Views
frank_m
Senior Contributor III

>...so we can switch to use LPC1769FBD100,551 and no need change firmware, right?

I think a re-build for the new MCU will be required.

0 Kudos
Reply

3,334 Views
RoyJ
Contributor I

Hello Frank,

So you means I can't use the same Hex file for the alternative? that's will be a problem for me.

0 Kudos
Reply

3,327 Views
frank_m
Senior Contributor III

You will need to try. Perhaps it works, but as other threads here show, there is a good chance it does not.

> that's will be a problem for me.

Could be worse. Perhaps you should have checked to projected lifetime more closely when planning for a project. My company has similar problems with Fujitsu stuff, only there is no similar and compatible replacement.

0 Kudos
Reply

3,346 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi RoyJ

These two parts are pin to pin replacement. no need change firmware as well.

The main differences are, LPC1769 has higher maximal CPU Frequency(120MHz) and larger memory size(512KB)

Have a nice day,

Jun Zhang

0 Kudos
Reply

3,333 Views
RoyJ
Contributor I

Hello Jennie,

Do we need to re-build the firmware when we change the MCU from LPC1766FBD100,551 to the alternative(LPC1769FBD100,551)?

0 Kudos
Reply

3,401 Views
frank_m
Senior Contributor III

That designations sound very similar, which lead me to believe you could expect an EOL message for this alternative type soon.

But you would need to contact NXP or an official distributor directly - this is not tha type of info given in a public forum like this.

0 Kudos
Reply