LPC1765 flash retention time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1765 flash retention time

ソリューションへジャンプ
1,896件の閲覧回数
davidouatt08
Contributor I

Hello,

I need to estimate the flash retention time for an LPC1765 constantly powered under a temperature of 40°C.

In the Reference Manual, the retention time for a powered device is 10 years min and 20years min for an unpowered device, but I look for a more precise estimation for a running without interruption at 40°C.

Support is much appreciated 

Regards

ラベル(1)
0 件の賞賛
返信
1 解決策
1,883件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

If the devices are using under all the specifications. those can support the 10 years at 40C, as you can see on the datasheet, this spec is from Tamb = −40 °C to +85 °C.

 

You need to be sure while you are running at 40C continuously all the other specs are under spec, also the power consumption, read and write on memories, etc.

 

I hope this will help you

Have a good day.

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,884件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

If the devices are using under all the specifications. those can support the 10 years at 40C, as you can see on the datasheet, this spec is from Tamb = −40 °C to +85 °C.

 

You need to be sure while you are running at 40C continuously all the other specs are under spec, also the power consumption, read and write on memories, etc.

 

I hope this will help you

Have a good day.

 

 

 

0 件の賞賛
返信