LPC1765 flash retention time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1765 flash retention time

Jump to solution
1,900 Views
davidouatt08
Contributor I

Hello,

I need to estimate the flash retention time for an LPC1765 constantly powered under a temperature of 40°C.

In the Reference Manual, the retention time for a powered device is 10 years min and 20years min for an unpowered device, but I look for a more precise estimation for a running without interruption at 40°C.

Support is much appreciated 

Regards

Labels (1)
0 Kudos
Reply
1 Solution
1,887 Views
vicentegomez
NXP TechSupport
NXP TechSupport

If the devices are using under all the specifications. those can support the 10 years at 40C, as you can see on the datasheet, this spec is from Tamb = −40 °C to +85 °C.

 

You need to be sure while you are running at 40C continuously all the other specs are under spec, also the power consumption, read and write on memories, etc.

 

I hope this will help you

Have a good day.

 

 

 

View solution in original post

0 Kudos
Reply
1 Reply
1,888 Views
vicentegomez
NXP TechSupport
NXP TechSupport

If the devices are using under all the specifications. those can support the 10 years at 40C, as you can see on the datasheet, this spec is from Tamb = −40 °C to +85 °C.

 

You need to be sure while you are running at 40C continuously all the other specs are under spec, also the power consumption, read and write on memories, etc.

 

I hope this will help you

Have a good day.

 

 

 

0 Kudos
Reply