LPC1756 short circuit problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1756 short circuit problem

1,933件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sathyan on Fri Mar 28 22:46:48 MST 2014
Hello!

I have brought two LPC1756 Microcontrollers. I tried to program the chip using the circuit in the attached file.

Unfortunately, the controller gets shorted whenever i supply 3.3V to it.

There is no short between any pins.

I couldn't find any reason for the short circuit, as i even tried connecting only the VDD and VSS pins to the 3.3V power supply.

Please help.

Regards,
C.Sathyan
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sathyan on Sun Mar 30 22:06:00 MST 2014
@LabRat, Yes you are right!

I soldered the chip in wrong orientation!

I desoldered the chip and reassembled it. Now It's working fine.

Thanks a lot.

-Sathyan
0 件の賞賛
返信

1,895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Sat Mar 29 02:21:04 MST 2014

Quote: sathyan
I have brought two LPC1756 Microcontrollers. I tried to program the chip using the circuit in the attached file.



Are you using a board, too?


Quote: sathyan
I couldn't find any reason for the short circuit, as i even tried connecting only the VDD and VSS pins to the 3.3V power supply.



Sounds like soldered in with wrong chip orientation...
0 件の賞賛
返信