LPC1752 SWD failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1752 SWD failure

1,605 Views
meirkatz
Contributor I

After programming the device I got memory error and then I can't re program the device using SWD or JTAG.  I tried to keep the device in RESET but it didn't work..

Please help 

Labels (1)
0 Kudos
Reply
1 Reply

1,505 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Meir Katz,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Whether you can share the error message when you try to program the LPC1752 chip, in further, did you try to force the LPC1752 to enter into the ISP mode?

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply