LPC1752 SWD failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1752 SWD failure

1,768件の閲覧回数
meirkatz
Contributor I

After programming the device I got memory error and then I can't re program the device using SWD or JTAG.  I tried to keep the device in RESET but it didn't work..

Please help 

ラベル(1)
0 件の賞賛
返信
1 返信

1,668件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Meir Katz,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Whether you can share the error message when you try to program the LPC1752 chip, in further, did you try to force the LPC1752 to enter into the ISP mode?

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信