LPC15xx SET_POWER API - what does this really control?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC15xx SET_POWER API - what does this really control?

2,147件の閲覧回数
nsmith17044
Contributor II

I'm trying to get an understanding of the 4 different set_power mode options in the LPC1518.  Per UM10736 (V1.1) page 584:

/* set_power mode options */
#define PWR_DEFAULT 0
#define PWR_CPU_PERFORMANCE 1
#define PWR_EFFICIENCY 2
#define PWR_LOW_CURRENT 3

Section 34.4.2.2 seems to elude to this effecting only the M3 core. The LPCOpen documenation nor the rom_pwr_15xx.h file in the LPCOpen library code is of any help.

I do see about a 1.5 to 2 mA reduction in consumption at 24MHz core speed between PWR_LOW_CURRENT and PWR_DEFAULT.  I would like to know what really is being effected.  Are any peripherals or bus behaviors effected?  Anyone have any experience with these settings?  Is there better documentation on this somewhere? 

ラベル(2)
2 返答(返信)

1,955件の閲覧回数
nsmith17044
Contributor II

Update: I found out (the hard way) that use of PWR_EFFICIENCY mode / profile appears to impact the IAP Chip_IAP_CopyRamToFlash() function.  With PWR_DEFAULT, the operation of that function works.  With PWR_EFFICIENCY the operation appears to be successful based on the response code, however the flash is not updated.  This is at a system frequency of 24MHz.

From that behavior I surmise that the power profile setting appears to effect the flash block some how.

1,955件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Nathan,

Please take a look to the following thread:

Power-saving 

Best Regards!
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信