LPC4370FET100において、外部シリアルパラレル変換(DS92LV2422)からの24bit幅データに対してDMAによる連続リードをする際に、21Mサンプル/秒でリードしようとしましたが、その半分の速度(10.5Mサンプル/秒)でしかCS信号が出力されませんでした。マイコン動作クロックは192MHzで動作させています。LPC4370FET100で、21Mサンプル/sでDMAによる連続リードする方法はないのでしょうか?また、LPC4370FET256でも同様でしょうか?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4370FET100において、外部シリアルパラレル変換(DS92LV2422)からの24bit幅データに対してDMAによる連続リードをする際に、21Mサンプル/秒でリードしようとしましたが、その半分の速度(10.5Mサンプル/秒)でしかCS信号が出力されませんでした。マイコン動作クロックは192MHzで動作させています。LPC4370FET100で、21Mサンプル/sでDMAによる連続リードする方法はないのでしょうか?また、LPC4370FET256でも同様でしょうか?

531 Views
taniguchi_shini
Contributor I

LPC4370FET100において、外部シリアルパラレル変換(DS92LV2422)からの24bit幅データに対してDMAによる連続リードをする際に、21Mサンプル/秒でリードしようとしましたが、その半分の速度(10.5Mサンプル/秒)でしかCS信号が出力されませんでした。マイコン動作クロックは192MHzで動作させています。LPC4370FET100で、21Mサンプル/sでDMAによる連続リードする方法はないのでしょうか?また、LPC4370FET256でも同様でしょうか?

0 Kudos
2 Replies

405 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

First of all, sorry for the later reply.

I had done a DMA performance test based on MCB4300 board with LPC4357 chip mounted, which with the same performance of LPC4370 DMA module.
The test using DMA channel 0 with source/destination transfer width word(32-bit) and source/destination burst size is 32.
Please check below test result:
Data transfer results [MODE: DMA]
=========================================
SOURCE  ADDR: 0x28100000
DESTN   ADDR: 0x28500000
XFER    SIZE: 2097152 (Bytes)
CPU    SPEED: 204.0 (MHz)
START   TIME: 547956208 (ticks)
END     TIME: 553271417 (ticks)
TIME   TAKEN: 26054 (uSec(s))
SRC/DST COMP: MATCHING

It will use 26054us to transfer 2097152 bytes from SDRAM memory 0x28100000 to SDRAM memory 0x28500000.
As a calculated result, LPC4357 DMA module will transfer 80.49M bytes per seconde.

From customer description, the LPC4370 will read the 24-bit data from external serial parallel conversion (DS92LV 2422), which module as LPC4370 and DS92LV2422 interface?
If customer is using External Memory Controller(EMC) as interface?
The LPC4370 DAM performance should match with customer requirement.
Then, it need to check the interface module speed.
If customer using the EMC as interface, if it is possible to provide the related connection schematics and related initialization code.
Thank you for the attention.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

405 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

can you please put your question in English.

Thanks

0 Kudos