LPC15xx ADC maximum sample rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC15xx ADC maximum sample rate

3,162 Views
martinlorenz
Contributor II

Hello,

I am just examining the ADC example code periph_adc of LPCXpresso for LPC1549 and I found a strange issue:

The example code uses

/* Setup for maximum ADC clock rate */

    Chip_ADC_SetClockRate(LPC_ADC0, ADC_MAX_SAMPLE_RATE);

which uses ADC_MAX_SAMPLE_RATE=50e6, the maximum ADC conversion rate of 50MHz for the 12bit ADC as given in the manual. So far so good, but stepping through the code reveals that this call translates into:

/* Set ADC clock rate */

void Chip_ADC_SetClockRate(LPC_ADC_T *pADC, uint32_t rate)

{

    uint32_t div;

 

    /* Get ADC clock source to determine base ADC rate. IN sychronous mode,

       the ADC base clock comes from the system clock. In ASYNC mode, it

       comes from the ASYNC ADC clock and this function doesn't work. */

    div = Chip_Clock_GetSystemClockRate() / rate;

    if (div == 0) {

        div = 1;

    }

 

    Chip_ADC_SetDivider(pADC, (uint8_t) div - 1);

}

and the divider is set to div=72e6/50e6=1. So actually, the ADC runs with an clock rate of 72MHz which is above the specified 50MHz maximum rate. I would have expected that the CPU clock of 72MHz is divided by 2 to get 36MHz which is below the maximum value.

 

Even more strange: The ADC seems to work quite well with 72MHz clock. I was sampling a 50kHz sinus signal with 72MHz/26=2.77MHz sample rate (one conversion takes 26 cycles and not 25 as given in the manual) and I got reasonable noise (on the least significant bit) and reasonable distortions/non-linearities (looking on the harmonics after FFT).

 

Dear NXP support, can you please state on this issue?

How safe is it to operate the ADC out of limits, as given in the example code?

Will the example code be corrected?

Or will the specification be corrected, if it is save to run the ADC with 72MHz?

 

Do other users have experience with operating the ADC with 72MHz clock rate?

 

Regards, Martin

 

Labels (2)
0 Kudos
Reply
3 Replies

2,547 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

We do recommend customer to use the LPC1549 ADC module with Max. ADC clock 50MHz.

We could not guarantee the LPC1549 ADC module performance if ADC clock exceed 50MHz, especially for long term working.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,547 Views
martinlorenz
Contributor II

Do NXP people read this forum?

I would be glad to hear a comment from them...

0 Kudos
Reply

2,547 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Martin,

This has been reported to the developers, thanks for reporting this!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply