LPC1549 - stock production data register?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1549 - stock production data register?

2,669件の閲覧回数
Nutshellpan
Contributor I

Hi, we are having a very strange problem with C_CAN module on a LPC1549 microcontroller. The messages are not recognized by other can devices but, if we use an old stock microcontroller (same model, on the same board) we don't have any issue. We found this problem on every device in our latest production, and we tried to resolder the uc in order to exclude a production mistake.

So we'd like to be able to identify the production of these defective microcontroller not only by the production numbers on the package but also by any register if possible. Does anybody knows if is it possible?

0 件の賞賛
返信
3 返答(返信)

2,642件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

By register you could obtain part ID and die revision. Please check image below from LPC15xx user manual.

FelipeGarcia_2-1634926205642.png

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

 

0 件の賞賛
返信

2,606件の閲覧回数
Nutshellpan
Contributor I

Thank you, but I already checked those registers and they are all the same on our devices.
We're searching for a stock production date or ID.

0 件の賞賛
返信

2,601件の閲覧回数
converse
Senior Contributor V

From the LPC15xx data sheet https://www.nxp.com/docs/en/data-sheet/LPC15XX.pdf

The LPC15xx devices typically have the following top-side marking for LQFP100 packages:

LPC15xxJxxx Xxxxxx xx xxxyywwxxx

The LPC15xx devices typically have the following top-side marking for LQFP64 packages:

LPC15xxJ Xxxxxx xx xxxyywwxxx

The LPC15xx devices typically have the following top-side marking for LQFP48 packages:

LPC15xxJ Xxxxxx Xxxyy wwxxx

Field ‘yy’ states the year the device was manufactured. Field ‘ww’ states the week the device was manufactured during that year.

0 件の賞賛
返信