LPC1549 fast fourier transform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1549 fast fourier transform

2,006 Views
emrebaltaci
Contributor I

hello,

can i use fft function from cmsis dsp library. this library contains fft function. in the internet i found this library for suitable for lpc 13xx and 17xx series. it is suitable my lpc expresso 1549.

thanks for helping...

Labels (1)
0 Kudos
Reply
1 Reply

1,835 Views
soledad
NXP Employee
NXP Employee

Hi,

Please try using the CMSIS DSP for cortex M3,

This may be helpful to you:

CMSIS DSP Library Support 

 

The library can be found in the Examples directory of the MCUXpresso install.

pastedImage_1.png


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply