LPC1549 blink darn you, blink!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1549 blink darn you, blink!

220 Views
DanielLongo
Contributor I

I have the LPC1549 on its own board and I am trying to get familiar with MCUExpresso by using the periph_blinky example. It builds and flashes successfully. Since it is not on the development board, I need to reassign the LED pins. It is clear in the systick.c file where the LED pins are set:

Board_LED_Set(0, false);

Board_LED_Set(1, true);

 

However, I can't find where the pins are defined. Where do I find where pins "0" and "1" are defined? I need to change them to PIO0_22 and PIO0_23.

Thanks!

0 Kudos
Reply
0 Replies