LPC1549 QEI POS and INXCNT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1549 QEI POS and INXCNT

2,040 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Thu Aug 27 21:47:03 MST 2015
Has anybody encounter the problem that the POS register never change and the actual position is reported in the INXCNT register instead? So where is the actual index count register?

I had no such problem with the QEI in LPC1768 for another project.

Sam
标签 (1)
0 项奖励
回复
3 回复数

1,906 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Aug 28 09:20:58 MST 2015

Quote: [email protected]
That's a very strange and unexpected behavior. The user manual is misleading too.



UM:

Quote:
22.6.2.2 QEI Maximum Position register
This register contains the maximum value of the encoder position.



So with MAXPOS  = 0, POS is counting from 0 to 0  :D 
0 项奖励
回复

1,906 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Fri Aug 28 09:08:06 MST 2015
Good call! Once I set the MAXPOS, POS reports correctly and INXCNT stays at 0. That's a very strange and unexpected behavior. The user manual is misleading too.

Thanks.
Sam.

22.6.2.6
22.6.2.7
22.6.2.8
22.6.2.9
QEI Index Count register
This register contains the current value of the encoder position. Increments or decrements when encoder counts occur, depending on the direction of rotation.
Table 306. QEI Index Count register (INXCNT, address 0x4005 8020) bit description
Bit Symbol Description Reset value
31:0 ENCPOS Current encoder position value. 0
0 项奖励
回复

1,906 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Aug 27 23:41:46 MST 2015

Quote: [email protected]
Has anybody encounter the problem that the POS register never change and the actual position is reported in the INXCNT register instead?



No :)

Did you set MAXPOS ?
0 项奖励
回复