LPC1549 - PINASSIGN15 - Reset Vaule of the Reserved fields

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1549 - PINASSIGN15 - Reset Vaule of the Reserved fields

1,344 次查看
pepoja
Contributor II

Hi,


Please LPC masters, If you have a few minutes of free time, have look to the reset value of the register PINASSIGN15.
In UM10736, page 136, Table122 you can find Reset value: 0xFFFF FFFF ( Reserved byte also), but if I was trying to read in real MCU (LPC1549JBD64) I got value 0x0000 FFFF - Reserved bytes are 0x00!

What is wrong? User's manual or chip?

Thak you.

标签 (1)
标记 (2)
2 回复数

1,181 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello,

Thanks a lot for your carefully review of the SFR reset value. In actual usage, we don't read the reserve bit, because it's contain is none of meanings, and contain value is not determined. In documentation, we just give a "1" to these bits, but this doesn't mean it be "1". For these bits, we need avoid to read or write them.

Have a great day, 

Victor.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,181 次查看
pepoja
Contributor II

... "1" to these bits, but this doesn't mean it be "1" ... - It's georgeous!

If "1" doesn't mean "1" and "1" is not "0", what's mean "1" ??

No, it's joke only :-)

For this reserved bits is better write in datasheet '-' as reset value. That's all.

It's only small mistake.

Have a nice day.