LPC1549 LPCXpresso board - Problem when connected with a serial terminal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1549 LPCXpresso board - Problem when connected with a serial terminal

2,543 Views
doini
Contributor III

Hello,

I am using LPCXpresso1549 demo board. I connect it to my PC with the LPCXpresso IDE and I can download and debug my code. I need to use a serial terminal (Tera Term) to display debugging messages. But I can use this ONLY after I download my code into the board through LPCXpresso IDE, while the board is still connected. After downloading, when I give the command "New Connection" from the serial terminal (Tera Term), it will appear: "COM4: LPC - LinkII UCom Port (COM4)" as a choice and I can connect my board to the serial terminal. So this is OK.
But, if I disconnect the board from the PC (disconnecting the USB cable), and then connect it again, I cannot display anything on the serial terminal. When I give the command "New Connection" from the serial terminal (Tera Term), it does not show the Port # where the LPCXpresso1549 demo board is plugged in. So I cannot choose the board for connecting to the serial terminal.
Also in the Device Manager the board appears now under "LPCDevice" as "LPC based USB device", whereas in the above situation after downloading, it appeared under "Ports (COM & LPT)" as "LPC - LinkII UCom Port (COM4)".
I need to use this board in a testing environment where there is not a computer having LPCXpresso IDE installed. So I need to download my code into the board through LPCXpresso IDE on my PC, take the board and use it with a serial terminal (Tera Term) on another computer in that testing environment, but I cannot use it because the board is not recognized by the serial terminal on that computer.
I would really appreciate any help!
Thank you,
Doini
0 Kudos
Reply
1 Reply

2,046 Views
lpcxpresso_supp
NXP Employee
NXP Employee

At the moment, the probe firmware is being soft loaded when you start a debug session by the IDE. For what you are trying to do, you need  pre-program the debug probe firmware into the onboard LPC-Link2's flash memory, using LPCScrypt.

For more details see:

Regards,

LPCXpresso Support

0 Kudos
Reply