LPC1549: How to use the DMA with the ADC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1549: How to use the DMA with the ADC

ソリューションへジャンプ
5,049件の閲覧回数
jespermadsen
Contributor III

I found this example:

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/DMA-Ping-Pong-application/ta-p/1120977

for the LPCXpressor54114 Board and changed it to match the  LPC1549 LPCXpresso™ board.

There are some ADC results in the buffer. But there are zeros and not compleately processed data there too.

I'm using the SCT2_Out3 to ADC0_SEQA to DMA. I'm not sure if the ADC_SEQA is setup correctly.

What could be wrong?

The code is shown below:

//-------------------------------------------------------------

#if defined (__USE_LPCOPEN)
#if defined(NO_BOARD_LIB)
#include "chip.h"
#else
#include "board.h"
#endif
#endif

#include <cr_section_macros.h>

#define NUM_BUFFERS 4
#define DMA_TRANSFER_SIZE 8
#define ADC_INPUT_CHANNEL 0

#define SCT_PWM_RATE 10000 /* PWM frequency 10 KHz */
#define SCT_PWM_PIN_OUT 3 /* COUT3 Generate square wave */
#define SCT_PWM_OUT 3 /* Index of OUT PWM */

uint16_t adcOut;

DMA_CHDESC_T ADC_TransferDescriptors[NUM_BUFFERS] __attribute__ ((aligned(512)));


uint16_t CapturedData[32];

uint16_t DMA_Sum=0;

/**
*
* ADC IRQ not Used right now... Only for testing
*/
void ADC_SEQA_IRQHandler(void)
{
/* If SeqA flags is set i.e. data in global register is valid then read it */
Chip_ADC_ClearFlags(LPC_ADC0,0xFFFFFFFF);
}


void DMA_IRQHandler(void)
{
static uint16_t DMA_Sum=0;

DMA_Sum++;

if(DMA_Sum ==8)
{
DMA_Sum=4;
}


/* Rrror interrupt on channel 0? */
if ((Chip_DMA_GetIntStatus(LPC_DMA) & DMA_INTSTAT_ACTIVEERRINT) != 0)
{
/* This shouldn't happen for this simple DMA example, so set the LED
to indicate an error occurred. This is the correct method to clear
an abort. */
Chip_DMA_DisableChannel(LPC_DMA, DMA_CH0);
while ((Chip_DMA_GetBusyChannels(LPC_DMA) & (1 << DMA_CH0)) != 0) {}
Chip_DMA_AbortChannel(LPC_DMA, DMA_CH0);
Chip_DMA_ClearErrorIntChannel(LPC_DMA, DMA_CH0);
Chip_DMA_EnableChannel(LPC_DMA, DMA_CH0);
}

/* Clear DMA interrupt for the channel */
Chip_DMA_ClearActiveIntAChannel(LPC_DMA, DMA_CH0);
}

 

 

/***
* ____ __ __ _
* | _ \| \/ | / \
* | | | | |\/| | / _ \
* | |_| | | | |/ ___ \
* |____/|_| |_/_/ \_\
* / ___| ___| |_ _ _ _ __
* \___ \ / _ \ __| | | | '_ \
* ___) | __/ |_| |_| | |_) |
* |____/ \___|\__|\__,_| .__/
* |_|
*/
void DMA_Setup(void)
{
DMA_CHDESC_T Initial_DMA_Descriptor;

ADC_TransferDescriptors[0].source = (uint32_t)&LPC_ADC0->SEQ_GDAT[0];
ADC_TransferDescriptors[1].source = (uint32_t)&LPC_ADC0->SEQ_GDAT[0];
ADC_TransferDescriptors[2].source = (uint32_t)&LPC_ADC0->SEQ_GDAT[0];
ADC_TransferDescriptors[3].source = (uint32_t)&LPC_ADC0->SEQ_GDAT[0];


ADC_TransferDescriptors[0].dest = DMA_ADDR(&CapturedData[(0+1)*DMA_TRANSFER_SIZE-1]);
ADC_TransferDescriptors[1].dest = DMA_ADDR(&CapturedData[(1+1)*DMA_TRANSFER_SIZE-1]);
ADC_TransferDescriptors[2].dest = DMA_ADDR(&CapturedData[(2+1)*DMA_TRANSFER_SIZE-1]);
ADC_TransferDescriptors[3].dest = DMA_ADDR(&CapturedData[(3+1)*DMA_TRANSFER_SIZE-1]);

//The initial DMA desciptor is the same as the 1st transfer descriptor. It
//Will link into the 2nd of the main descriptors.

ADC_TransferDescriptors[0].next = (uint32_t)&ADC_TransferDescriptors[1];
ADC_TransferDescriptors[1].next = (uint32_t)&ADC_TransferDescriptors[2];
ADC_TransferDescriptors[2].next = (uint32_t)&ADC_TransferDescriptors[3];

//Link back to the 1st descriptor
ADC_TransferDescriptors[3].next = (uint32_t)&ADC_TransferDescriptors[0];

//For a test, stop the transfers here. The sine wave will look fine.
//ADC_TransferDescriptors[3].next = 0;

ADC_TransferDescriptors[0].xfercfg = (DMA_XFERCFG_CFGVALID |
DMA_XFERCFG_RELOAD |
DMA_XFERCFG_SETINTA |
DMA_XFERCFG_WIDTH_16 |
DMA_XFERCFG_SRCINC_0 |
DMA_XFERCFG_DSTINC_1 |
DMA_XFERCFG_XFERCOUNT(DMA_TRANSFER_SIZE));

ADC_TransferDescriptors[1].xfercfg = ADC_TransferDescriptors[0].xfercfg;
ADC_TransferDescriptors[2].xfercfg = ADC_TransferDescriptors[0].xfercfg;

ADC_TransferDescriptors[3].xfercfg = (DMA_XFERCFG_CFGVALID |
DMA_XFERCFG_RELOAD |
DMA_XFERCFG_SETINTA |
DMA_XFERCFG_WIDTH_16 |
DMA_XFERCFG_SRCINC_0 |
DMA_XFERCFG_DSTINC_1 |
DMA_XFERCFG_XFERCOUNT(DMA_TRANSFER_SIZE));

Initial_DMA_Descriptor.source = ADC_TransferDescriptors[0].source;
Initial_DMA_Descriptor.dest = ADC_TransferDescriptors[0].dest;
Initial_DMA_Descriptor.next = (uint32_t)&ADC_TransferDescriptors[1];
Initial_DMA_Descriptor.xfercfg = ADC_TransferDescriptors[0].xfercfg;

/* DMA initialization - enable DMA clocking and reset DMA if needed */
Chip_DMA_Init(LPC_DMA);

/* Enable DMA controller and use driver provided DMA table for current descriptors */
Chip_DMA_Enable(LPC_DMA);
Chip_DMA_SetSRAMBase(LPC_DMA, DMA_ADDR(Chip_DMA_Table));

/* Setup channel 0 for the following configuration:
- High channel priority
- Interrupt A fires on descriptor completion */
Chip_DMA_EnableChannel(LPC_DMA, DMA_CH0);
Chip_DMA_EnableIntChannel(LPC_DMA, DMA_CH0);
Chip_DMA_SetupChannelConfig(LPC_DMA, DMA_CH0, //(DMA_CFG_PERIPHREQEN |
(DMA_CFG_HWTRIGEN |
DMA_CFG_TRIGBURST_BURST |
DMA_CFG_TRIGTYPE_EDGE |
DMA_CFG_TRIGPOL_HIGH | //DMA_CFG_TRIGPOL_HIGH
DMA_CFG_BURSTPOWER_1 |
DMA_CFG_CHPRIORITY(0)
)
);


//make sure ADC Sequence A interrupts is selected for for a DMA trigger
Chip_INMUX_SetDMATrigger(DMA_CH0, DMATRIG_ADC0_SEQA_IRQ);

/* Enable DMA interrupt */
NVIC_EnableIRQ(DMA_IRQn);

// The 1st descriptor is set up through the registers.

/* Setup transfer descriptor and validate it */
Chip_DMA_SetupTranChannel(LPC_DMA, DMA_CH0, &Initial_DMA_Descriptor);

//Use the transfer configuration for our 4 main descriptors
Chip_DMA_SetupChannelTransfer(LPC_DMA, DMA_CH0, ADC_TransferDescriptors[0].xfercfg);
Chip_DMA_SetValidChannel(LPC_DMA, DMA_CH0);
}

void SCT_PWM_Generate(void)
{
/* Initialize the SCT2 as PWM and set frequency */
Chip_SCTPWM_Init(LPC_SCT2);
Chip_SCTPWM_SetRate(LPC_SCT2, SCT_PWM_RATE);

/* Use SCT2_OUT3 pin */
Chip_SCTPWM_SetOutPin(LPC_SCT2, SCT_PWM_OUT, SCT_PWM_PIN_OUT);

/* Start with 50% duty cycle */
Chip_SCTPWM_SetDutyCycle(LPC_SCT2, SCT_PWM_OUT, Chip_SCTPWM_PercentageToTicks(LPC_SCT2, 50));
Chip_SCTPWM_Start(LPC_SCT2);
}


/***
* _ ____ ____
* / \ | _ \ / ___|
* / _ \ | | | | |
* / ___ \| |_| | |___
* /_/__ \_\____/ \____|
* / ___| ___| |_ _ _ _ __
* \___ \ / _ \ __| | | | '_ \
* ___) | __/ |_| |_| | |_) |
* |____/ \___|\__|\__,_| .__/
* |_|
*/
void ADC_Setup(void)
{
/*Set Asynch Clock to the Main clock*/
// LPC_SYSCON->ADCCLKSEL = 0;
// Chip_Clock_SetADCASYNCSource(SYSCTL_ADCASYNCCLKSRC_IRC);
//Set the divider to 1 and enable. note, the HALT bit (30) and RESET (29) are not in the manual
// LPC_SYSCON->ADCCLKDIV = 0;

/* Initialization ADC to 12 bit and set clock divide to 1 to operate synchronously at System clock */
Chip_ADC_Init(LPC_ADC0, ADC_CR_BITACC(0) | ADC_CR_CLKDIV(0)| ADC_CR_ASYNMODE);
Chip_ADC_SetClockRate(LPC_ADC0, ADC_MAX_SAMPLE_RATE);
//select ADC Channel 0 as input
Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 8, IOCON_FUNC0 | IOCON_MODE_INACT | IOCON_ADMODE_EN);
Chip_SWM_Init();
Chip_SWM_EnableFixedPin(SWM_FIXED_ADC0_0); //P0_8

Chip_ADC_SetADC0Input(LPC_ADC0, ADC_INSEL_ADC0);

//Setup ADC0_SEQA_IRQ
Chip_ADC_SetupSequencer(LPC_ADC0,ADC_SEQA_IDX,
ADC_SEQ_CTRL_SEQ_ENA |
ADC_SEQ_CTRL_CHANSEL(ADC_INPUT_CHANNEL) |
ADC0_SEQ_CTRL_HWTRIG_SCT2_OUT3 |
// ADC_SEQ_CTRL_HWTRIG_POLPOS |
// ADC_SEQ_CTRL_HWTRIG_SYNCBYPASS |
ADC_SEQ_CTRL_MODE_EOS);
/* Enable Sequence A interrupt */
Chip_ADC_EnableInt(LPC_ADC0, ADC_INTEN_SEQA_ENABLE);

/* Calibrate ADC */
Chip_ADC_StartCalibration(LPC_ADC0);
while (!(Chip_ADC_IsCalibrationDone(LPC_ADC0))) {}

Chip_ADC_ClearFlags(LPC_ADC0, Chip_ADC_GetFlags(LPC_ADC0));
// Chip_ADC_EnableInt(LPC_ADC0, ADC_INTEN_SEQA_ENABLE);
// NVIC_EnableIRQ(ADC0_SEQA_IRQn);
Chip_ADC_EnableSequencer(LPC_ADC0, ADC_SEQA_IDX);

}

int main(void)
{

/* Setup SystemCoreClock and any needed board code */
SystemCoreClockUpdate();
Board_Init();

DMA_Setup();
ADC_Setup();
SCT_PWM_Generate();


while(1)
{}
}

0 件の賞賛
返信
1 解決策
5,044件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jesper,

“There are some ADC results in the buffer. But there are zeros and not completely processed data there too.”

-> Dose the data all right when only use ADC,without DMA?

 

BR

Alice

元の投稿で解決策を見る

5 返答(返信)
5,045件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jesper,

“There are some ADC results in the buffer. But there are zeros and not completely processed data there too.”

-> Dose the data all right when only use ADC,without DMA?

 

BR

Alice

5,020件の閲覧回数
jespermadsen
Contributor III

Hello Alice.

Now the values comes into the buffer.. Thanks.

I removed the boardlib and made some small changes:

#include "chip.h"

#include <cr_section_macros.h>

#define NUM_BUFFERS 4
#define DMA_TRANSFER_SIZE 8
#define ADC_INPUT_CHANNEL 0

#define SCT_PWM_RATE   10000          /* PWM frequency 10 KHz */
#define SCT_PWM_PIN_OUT    3          /* COUT3 Generate square wave */
#define SCT_PWM_OUT        3          /* Index of OUT PWM */

uint16_t adcOut;

DMA_CHDESC_T ADC_TransferDescriptors[NUM_BUFFERS] __attribute__ ((aligned(512)));


uint16_t CapturedData[32];

uint16_t DMA_Sum=0;

/**
 *
 * ADC IRQ not Used right now... Only for testing
 */
void ADC_SEQA_IRQHandler(void)
{
            /* If SeqA flags is set i.e. data in global register is valid then read it */
        Chip_ADC_ClearFlags(LPC_ADC0,0xFFFFFFFF);
}


void DMA_IRQHandler(void)
{
        static uint16_t DMA_Sum=0;

        DMA_Sum++;

         if(DMA_Sum ==8)
         {
           DMA_Sum=4;
         }


     /* Error interrupt on channel 0? */
     if ((Chip_DMA_GetIntStatus(LPC_DMA) & DMA_INTSTAT_ACTIVEERRINT) != 0)
     {
          /* This shouldn't happen for this simple DMA example, so set the LED
             to indicate an error occurred. This is the correct method to clear
             an abort. */
          Chip_DMA_DisableChannel(LPC_DMA, DMA_CH0);
          while ((Chip_DMA_GetBusyChannels(LPC_DMA) & (1 << DMA_CH0)) != 0) {}
          Chip_DMA_AbortChannel(LPC_DMA, DMA_CH0);
          Chip_DMA_ClearErrorIntChannel(LPC_DMA, DMA_CH0);
          Chip_DMA_EnableChannel(LPC_DMA, DMA_CH0);
     }

     /* Clear DMA interrupt for the channel */
	Chip_DMA_ClearActiveIntAChannel(LPC_DMA, DMA_CH0);
}





     /***
      *      ____  __  __    _
      *     |  _ \|  \/  |  / \
      *     | | | | |\/| | / _ \
      *     | |_| | |  | |/ ___ \
      *     |____/|_|  |_/_/   \_\
      *     / ___|  ___| |_ _   _ _ __
      *     \___ \ / _ \ __| | | | '_ \
      *      ___) |  __/ |_| |_| | |_) |
      *     |____/ \___|\__|\__,_| .__/
      *                          |_|
      */
void DMA_Setup(void)
{
        DMA_CHDESC_T Initial_DMA_Descriptor;

     ADC_TransferDescriptors[0].source = (uint32_t)&LPC_ADC0->SEQ_GDAT[0];
     ADC_TransferDescriptors[1].source = (uint32_t)&LPC_ADC0->SEQ_GDAT[0];
     ADC_TransferDescriptors[2].source = (uint32_t)&LPC_ADC0->SEQ_GDAT[0];
     ADC_TransferDescriptors[3].source = (uint32_t)&LPC_ADC0->SEQ_GDAT[0];


     ADC_TransferDescriptors[0].dest = DMA_ADDR(&CapturedData[(0+1)*DMA_TRANSFER_SIZE-1]);
     ADC_TransferDescriptors[1].dest = DMA_ADDR(&CapturedData[(1+1)*DMA_TRANSFER_SIZE-1]);
     ADC_TransferDescriptors[2].dest = DMA_ADDR(&CapturedData[(2+1)*DMA_TRANSFER_SIZE-1]);
     ADC_TransferDescriptors[3].dest = DMA_ADDR(&CapturedData[(3+1)*DMA_TRANSFER_SIZE-1]);

     //The initial DMA desciptor is the same as the 1st transfer descriptor.   It
     //Will link into the 2nd of the main descriptors.

     ADC_TransferDescriptors[0].next = (uint32_t)&ADC_TransferDescriptors[1];
     ADC_TransferDescriptors[1].next = (uint32_t)&ADC_TransferDescriptors[2];
     ADC_TransferDescriptors[2].next = (uint32_t)&ADC_TransferDescriptors[3];

     //Link back to the 1st descriptor
     ADC_TransferDescriptors[3].next = (uint32_t)&ADC_TransferDescriptors[0];

     //For a test,  stop the transfers here.   The sine wave will look fine.
     //ADC_TransferDescriptors[3].next = 0;

     ADC_TransferDescriptors[0].xfercfg = (DMA_XFERCFG_CFGVALID |
                               DMA_XFERCFG_RELOAD  |
                               DMA_XFERCFG_SETINTA |
                               DMA_XFERCFG_WIDTH_16 |
                               DMA_XFERCFG_SRCINC_0 |
                               DMA_XFERCFG_DSTINC_1 |
                               DMA_XFERCFG_XFERCOUNT(DMA_TRANSFER_SIZE));

     ADC_TransferDescriptors[1].xfercfg = ADC_TransferDescriptors[0].xfercfg;
     ADC_TransferDescriptors[2].xfercfg = ADC_TransferDescriptors[0].xfercfg;

     ADC_TransferDescriptors[3].xfercfg = (DMA_XFERCFG_CFGVALID |
                               DMA_XFERCFG_RELOAD  |
                               DMA_XFERCFG_SETINTA |
                              DMA_XFERCFG_WIDTH_16 |
                              DMA_XFERCFG_SRCINC_0 |
                              DMA_XFERCFG_DSTINC_1 |
                              DMA_XFERCFG_XFERCOUNT(DMA_TRANSFER_SIZE));

     Initial_DMA_Descriptor.source = ADC_TransferDescriptors[0].source;
     Initial_DMA_Descriptor.dest =   ADC_TransferDescriptors[0].dest;
     Initial_DMA_Descriptor.next =  (uint32_t)&ADC_TransferDescriptors[1];
     Initial_DMA_Descriptor.xfercfg = ADC_TransferDescriptors[0].xfercfg;

     /* DMA initialization - enable DMA clocking and reset DMA if needed */
     Chip_DMA_Init(LPC_DMA);

     /* Enable DMA controller and use driver provided DMA table for current descriptors */
     Chip_DMA_Enable(LPC_DMA);
     Chip_DMA_SetSRAMBase(LPC_DMA, DMA_ADDR(Chip_DMA_Table));

     /* Setup channel 0 for the following configuration:
        - High channel priority
        - Interrupt A fires on descriptor completion */
     Chip_DMA_EnableChannel(LPC_DMA, DMA_CH0);
     Chip_DMA_EnableIntChannel(LPC_DMA, DMA_CH0);
     Chip_DMA_SetupChannelConfig(LPC_DMA, DMA_CH0,     //(DMA_CFG_PERIPHREQEN     |
                                   (DMA_CFG_HWTRIGEN        |
                                    DMA_CFG_TRIGBURST_BURST |
                                    DMA_CFG_TRIGTYPE_EDGE   |
                                    DMA_CFG_TRIGPOL_HIGH  |    //DMA_CFG_TRIGPOL_HIGH
                                    DMA_CFG_BURSTPOWER_1    |
                                    DMA_CFG_CHPRIORITY(0)
                                    )
                                    );


     //make sure ADC Sequence A interrupts is selected for for a DMA trigger
     Chip_INMUX_SetDMATrigger(DMA_CH0, DMATRIG_ADC0_SEQA_IRQ);

     /* Enable DMA interrupt */
     NVIC_EnableIRQ(DMA_IRQn);

     // The 1st descriptor is set up through the registers.

     /* Setup transfer descriptor and validate it */
     Chip_DMA_SetupTranChannel(LPC_DMA, DMA_CH0, &Initial_DMA_Descriptor);

     //Use the transfer configuration for our 4 main descriptors
     Chip_DMA_SetupChannelTransfer(LPC_DMA, DMA_CH0,     ADC_TransferDescriptors[0].xfercfg);
     Chip_DMA_SetValidChannel(LPC_DMA, DMA_CH0);
}

void SCT_PWM_Generate(void)
{
     /* Initialize the SCT2 as PWM and set frequency */
     Chip_SCTPWM_Init(LPC_SCT2);
     Chip_SCTPWM_SetRate(LPC_SCT2, SCT_PWM_RATE);

     /* Use SCT2_OUT3 pin */
     Chip_SCTPWM_SetOutPin(LPC_SCT2, SCT_PWM_OUT, SCT_PWM_PIN_OUT);

     /* Start with 50% duty cycle */
     Chip_SCTPWM_SetDutyCycle(LPC_SCT2, SCT_PWM_OUT, Chip_SCTPWM_PercentageToTicks(LPC_SCT2, 50));
     Chip_SCTPWM_Start(LPC_SCT2);
}


     /***
           *         _    ____   ____
           *        / \  |  _ \ / ___|
           *       / _ \ | | | | |
           *      / ___ \| |_| | |___
           *     /_/__ \_\____/ \____|
           *     / ___|  ___| |_ _   _ _ __
           *     \___ \ / _ \ __| | | | '_ \
           *      ___) |  __/ |_| |_| | |_) |
           *     |____/ \___|\__|\__,_| .__/
           *                          |_|
           */
void ADC_Setup(void)
{
     /* Initialization ADC to 12 bit and set clock divide to 1 to operate synchronously at System clock */
    Chip_ADC_Init(LPC_ADC0, ADC_CR_BITACC(0) | ADC_CR_CLKDIV(0)| ADC_CR_ASYNMODE);
	Chip_ADC_SetClockRate(LPC_ADC0, ADC_MAX_SAMPLE_RATE);
    //select ADC Channel 0 as input
    Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 8, IOCON_FUNC0 | IOCON_MODE_INACT | IOCON_ADMODE_EN);

    Chip_SWM_Init();
	Chip_SWM_EnableFixedPin(SWM_FIXED_ADC0_0);	//P0_8

    Chip_ADC_SetADC0Input(LPC_ADC0, ADC_INSEL_ADC0);

    //Setup ADC0_SEQA_IRQ
    Chip_ADC_SetupSequencer(LPC_ADC0,ADC_SEQA_IDX,
                              ADC_SEQ_CTRL_SEQ_ENA |
                              ADC_SEQ_CTRL_CHANSEL(ADC_INPUT_CHANNEL) |
                              ADC0_SEQ_CTRL_HWTRIG_SCT2_OUT3 |
//                              ADC_SEQ_CTRL_HWTRIG_POLPOS |
//                              ADC_SEQ_CTRL_HWTRIG_SYNCBYPASS |
                              ADC_SEQ_CTRL_MODE_EOS);

    /* Enable Sequence A interrupt */
	Chip_ADC_EnableInt(LPC_ADC0, ADC_INTEN_SEQA_ENABLE);

	/* Calibrate ADC */
	Chip_ADC_SetTrim(LPC_ADC0, ADC_TRIM_VRANGE_HIGHV);
	Chip_ADC_StartCalibration(LPC_ADC0);
	while (!(Chip_ADC_IsCalibrationDone(LPC_ADC0))) {}

	Chip_ADC_ClearFlags(LPC_ADC0, Chip_ADC_GetFlags(LPC_ADC0));
//	NVIC_EnableIRQ(ADC0_SEQA_IRQn);
	Chip_ADC_EnableSequencer(LPC_ADC0, ADC_SEQA_IDX);

}

int main(void) {
    // Read clock settings and update SystemCoreClock variable
    SystemCoreClockUpdate();

	Chip_GPIO_Init(LPC_GPIO);
	Chip_GPIO_SetPinDIROutput(LPC_GPIO, 0, 0);

    DMA_Setup();
    ADC_Setup();
    SCT_PWM_Generate();


    while(1)
    {}
    return 0 ;
}

 

0 件の賞賛
返信
5,038件の閲覧回数
jespermadsen
Contributor III

Hello Alice

If I keep a breakpoint in the loop and break it every time the interrupt fires, the value is not updated.

But if the MCU runs free for a while, and then I stop it, the value is correct.

Maybe the ADC interrupt is not correctly setup?

Best regards

Jesper

0 件の賞賛
返信
5,024件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

"Maybe the ADC interrupt is not correctly setup?"

-> No, when you use breakpoint, there is some delay by software.

I recommend you set block to lock problem, for example without DMA, just check whether ADC

, then add DMA...

 

4,990件の閲覧回数
jespermadsen
Contributor III

There are still some problems in the program.

I tried to set it up with

DMA_TRANSFER_SIZE 64

SCT_PWM_RATE 5000

And a 70 Hz triangle signal on the ADC-input.

The samples with DMA are chopped as you see in the pictures

The samples without DMA has only one jump.

How can this be?

PS: The curves in the figurs are not in fase.

ADC-input:

ADC_input.png

Samples without DMA:

ADC_samples_no_DMA.png

Samples with DMA:

ADC_samples.png

0 件の賞賛
返信