LPC1518 XTALIN specification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1518 XTALIN specification

1,002 次查看
masahirokiniwa
Contributor IV

At external clock for the oscillator slave mode, its data sheet was written the specification as below.

But it doesn't define the base or threshold voltage of its specification.

I think that the base voltage is center of min/max voltage and their thresholds are +/-140mV from center because it needs swing voltage min 280mV.

Could you tell me which voltage is the base/threshold?

pastedImage_3.png

pastedImage_1.png

Best regards,

M.Kiniwa

标签 (1)
0 项奖励
回复
0 回复数