LPC1518 XTALIN specification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1518 XTALIN specification

1,039件の閲覧回数
masahirokiniwa
Contributor IV

At external clock for the oscillator slave mode, its data sheet was written the specification as below.

But it doesn't define the base or threshold voltage of its specification.

I think that the base voltage is center of min/max voltage and their thresholds are +/-140mV from center because it needs swing voltage min 280mV.

Could you tell me which voltage is the base/threshold?

pastedImage_3.png

pastedImage_1.png

Best regards,

M.Kiniwa

ラベル(1)
0 件の賞賛
返信
0 返答(返信)