LPC1347 Not starting program

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1347 Not starting program

2,309 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Chill0309 on Fri Oct 12 14:01:00 MST 2012
I have a prototype LPC1347 which I can program and debug fine using CrossStudio. The application runs when I start debugging, but if I disconnect my SWD cable and power cycle it doesn't run the program from Flash. If I reconnect the SWD cable and start the application manually from CrossStudio without re-programming it starts fine.

Anyone any ideas what I'm missing.

I've got the reset line tied high and have toggled it low to force a restart.
标签 (1)
0 项奖励
回复
2 回复数

2,279 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Chill0309 on Sat Oct 13 00:37:45 MST 2012
Solved it.

https://rowley.zendesk.com/entries/251134-application-not-starting-up-from-reset-lpc1000
0 项奖励
回复

2,279 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Chill0309 on Fri Oct 12 14:14:48 MST 2012
.
0 项奖励
回复