LPC1343 is not enumerated as USB Mass Storage device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1343 is not enumerated as USB Mass Storage device

1,250 Views
sivaprakash16
Contributor I

usbConn.png

When switch S1 pressed, Driver is it is trying to connect the LPC 1343 as USB MSD. Installed USB sniffer and watched what is happening. PC is sending some bytes of data to lpc1343. But lpc1343 is not responding back to pc(Win 7). After some time Driver installation is failed and it says error(10) Device cannot start.  I tested all the hardware components. Looks like everything works properly.

Do i nedd to replace the Microcontroller? Please help me to solve this.

Thanks in advance. 

Labels (2)
0 Kudos
Reply
0 Replies