LPC54606 Deep Sleep, Utick0 interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54606 Deep Sleep, Utick0 interrupt

1,518 Views
santosh1
Contributor III

Hello, 

I am trying to wakeup a LPC54606 from deep sleep using utick0 timer. Here are the snippets of my initialization.

#define EXCLUDE_FROM_DEEPSLEEP (SYSCON_PDRUNCFG_PDEN_SRAMX_MASK|\
SYSCON_PDRUNCFG_PDEN_SRAM0_MASK|SYSCON_PDRUNCFG_PDEN_SRAM1_2_3_MASK| \
SYSCON_PDRUNCFG_PDEN_WDT_OSC_MASK)

// I am calling POWER_EnterDeepSleep with the above exclude mask. 

POWER_EnterDeepSleep(EXCLUDE_FROM_DEEPSLEEP);

Here is the micro-tick related initialization:

// Setup wake pin.
SYSCON->STARTERSET[0] |= SYSCON_STARTER_UTICK_MASK; /* GPIO pin interrupt 0 wake-up. */
EnableDeepSleepIRQ(UTICK0_IRQn);

utick0 is initialized using the fsl interface functions. 

I am toggling an LED in the IRQ handler - i can see the current consumption dropping - but i was expecting the LED to still toggle after the controller has gone into low power. And of course, i never come out of the low power mode at all.

Would appreciate any pointers on where the configuration is going wrong.

Thanks

Labels (1)
0 Kudos
Reply
0 Replies