LPC1317 peripheral on almost any pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC1317 peripheral on almost any pins

跳至解决方案
2,401 次查看
MJ1
Contributor I

Hi

Is possible to reconnect/repin peripherals on LPC1317 HVQFN33 package to pins which are not intended in manual for that peripheral? I.e. UART/USART RXD, TDX signals to SPI MOSI, MISO - PIO0_21, PIO0_22 pins?

 

Thanks

标签 (1)
0 项奖励
回复
1 解答
2,392 次查看
frank_m
Senior Contributor III

No.

Just like with the power supply and clock oscillator pins, the peripheral switch matrix options per pin are defined by the silicon. The possible configuration options per pin are given in the datasheet.

Alternatively, you could use a larger package, or implement some functionality by "bit-banging" (like a "software UART").

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,393 次查看
frank_m
Senior Contributor III

No.

Just like with the power supply and clock oscillator pins, the peripheral switch matrix options per pin are defined by the silicon. The possible configuration options per pin are given in the datasheet.

Alternatively, you could use a larger package, or implement some functionality by "bit-banging" (like a "software UART").

0 项奖励
回复
2,390 次查看
MJ1
Contributor I

Thanks so much.

0 项奖励
回复